Hello,
I am using custom board which is similar to the LCDKC6748. My DSP is running on 300MHz by external 25MHz crystal.
I have hard time to communicate with the PHY as i have kept preamble bit to 0 (Standard preamble) and CLDDIV to 50 as i am using input freq. is 50MHZ( for RMII) where as output is 1 MHZ.
After these i am settting MDIO_Enable in Control register and waiting for 5000 cycles. However, MDIO ALIVE register is always 0 means no PHYs detected.
Do i need to set any clock for the MDIO in .gel file in bootloader?
Do i need to make any special setting except set bit for CFGCHIP3 register for RMII_SEL bit.
Please guide me if you have any experience with it.
Thanks!