I am attempting to download and install the latest version of CCS (CCSv6). The download seems to work and then I rename the downloaded file from "ccs_setup_win32" to "ccs_setup_win32.exe". When I double click on this file it attempts to run but fails immediately with the following error message:
"Installer payload initialization failed. This is likely due to an incomplete or corrupt downloaded file."
I have tried this entire download/execute sequence several times with the same result each time.
Any suggestions?
Vic M.