Hi,
I am trying to initialize the VPIF for 10bit raw capture mode using the instructions in the tech ref and I have a few questions regarding some of the registers I have to configure. On page 1715 of the tech ref it says that I would need to configure the storage memory address control related registers.
Does "storage memory address registers" refer to these top and bottom field registers as shown in the figure below?
If yes, then is there any where that provides information of what these address registers are and what do they refer to? While the tech ref does provide examples for these address registers , seems to be a summary for experience individuals.
I am pretty new to interfacing image sensors and in my limited understanding for 8bit raw data, I have to program only the C0LUMA register but for 10bit raw data I have to program both the C0TLUMA and C0BLUMA registers. Can I just point both to the same address starting point or do I have to point them both to different starting address locations?
Regards,
Jerome Lieow