Hello All,
I have a problem with DSPF_sp_mat_mul(.asm) function in C674x_dsplib. The version is 1.03.00.01.
DSP : C6747
When we use this function to mix multiple audio source to multiple output, it works correctly for first 10 to 15 sec. But after that, the function always stops and the entire DSP program also stops(including SYSBIOS). It happens regardless of matrix size, it happens with 4x4 matrices multiplication.
It seems a bug, and we guess that there is a problem of memory usage. it looks like the function might be crashing the unexpected memory area.
Attached image is a log information on CCS, though it is a bit old information.
Could you check the function and advise me?
Thank you.
Best regards,
Shitnaro