This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

image processing on dsk6713

sir,

i want to connect vm3224k2 daughter card to dsk6713.i would like to know how to configure the daughtercard and a sample program  of video loop back that can run on ccsv5/6 and the videoto be displayed on lcd screen.

  • Hello,
    I will move your post to the appropriate device forum where the experts there can help you best.

    Thanks
    ki
  • Hi,

    Thanks for your post.

    With the VM3224K board removed from the DSK6713, can you build, load, and run example programs that came with the DSK6713?

    If you do not have any of those, you can go to the DSK board manufacturer's website

    www.spectrumdigital.com

    and find the support page for the DSK6713. Or you can go to the TI Wiki Pages and search for c6713 workshop to find the C6x1x workshop that includes some labs you can run while learning to use this board.

    Once you have run some of those example programs to confirm that the DSK6713 board is working properly, please contact the manufacturer of the VM3224K board for help with using the VM3224K board.

    Thanks & regards,

    Sivaraj K

    ----------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.

    ----------------------------------------------------------------------------------------------------------