Dear friends,
I bought a board of C6748 LCDK, and I want use Mcbsp. I don't find the sample code.Help........
Haidong Qiu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi user4730642,
You can see the McBSP examples in the following link.
C:\ti\pdk_OMAPL138_1_01_00_02\packages\ti\drv\exampleProjects\MCBSP_DigLpbkExampleProject
C:\ti\pdk_OMAPL138_1_01_00_02\packages\ti\drv\exampleProjects\MCBSP_MasterExampleProject
C:\ti\pdk_OMAPL138_1_01_00_02\packages\ti\drv\exampleProjects\MCBSP_SlaveExampleProject
You need to install the MCSDK package for OMAPL138 to get this "pdk_OMAPL138_1_01_00_02" .
processors.wiki.ti.com/.../MCSDK_OMAPL138_User_Guide_Chapter_Exploring
software-dl.ti.com/.../index_FDS.html
Hi,
Thanks for your post.
We do not have McBSP Starterware/CSL examples for C6748 instead there are existing examples for McBSP from BIOSPSP examples and you can download the same from the below:
http://software-dl.ti.com/dsps/dsps_registered_sw/sdo_sb/targetcontent/psp/bios_psp/index.html
After installing BIOS PSP 1.30.00 , you could see the McBSP DSP BIOS example on the below path:
~\BIOSPSP\packages\ti\pspiom\examples\evm6748\mcbsp\build\ccs4\master\.ccsproject
The other one is from BIOS PSP 03.00.01 which is a SYSBIOS McBSP example and you could download the same from the below page:
http://software-dl.ti.com/dsps/dsps_public_sw/psp/BIOSPSP/index.html
After installing BIOS PSP 03.00.01, you could find the McBSP master example from the PDK directory as shown in the path below:
~\pdk_C6748_2_0_0_0\biospsp_03_00_01\drivers\examples\evm6748\mcbsp\Master\src
Thanks & regards,
Sivaraj K
----------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
----------------------------------------------------------------------------------------------------------