I am presently work on Tms320c6713 Dsk Eval Board. I have already used GPIO pin (1,2,3 & 8,9,10,11,12,13,14,15) as a input/output.
Now i also need to use GPIO pin(4,5,6,7) , these are assigned for GPIO interupt pins. For my present project work, i need total 14 GPIO pins for general input/output. But i can use only 11 pins. There have four more GPIO interrupt pins [GPIO pin(4,5,6,7)]. But i don't know, how to use this pins as a general input/output.
If any body know the solution , kindly inform me please.