I am attempting to add NDK support to an existing application using the procedure from the NDK 2.25 User's Guide however when I build the application there are a number of unresolved symbols (NDK_accept, NDK_bind, etc). I am using BSD sockets. Clearly I need to link to the library containing these routines however I don't know where that may be. I am using Version: 6.1.1.00022 of CCS and the ti-cgt-c6000_8.1.0 compiler.
Here's the error message:
Here's the configuration: