Hi,
I am trying to build biospsp_03_00_01_00, have installed all of the required libraries and set the environment variables. When I try to build, I get the following error:
C:\temp\ti\biospsp_03_00_01_00>gmake all
# Configuring XDC packages for cslr_evm6748_example_uart:c6xdsp:debug
gmake -C C:/temp/ti/cslr\evm6748\examples\uart xdc_configuro PLATFORM=c6748-evm
CORE=c6xdsp PROFILE_c6xdsp=debug
gmake[1]: Entering directory `C:/temp/ti/cslr/evm6748/examples/uart'
# Invoking configuro...
a+x maketemp_configuro_cmd_c6xdsp.bat
maketemp_configuro_cmd_c6xdsp.bat
make (e=-1): Error -1
gmake[1]: *** [xdc_configuro] Error -1
gmake[1]: Leaving directory `C:/temp/ti/cslr/evm6748/examples/uart'
gmake: *** [cslr_evm6748_example_uart] Error 2
Any ideas what the cause of the error might be?
Thanks
Brian