Hi all,
Because of optimizing my source code by using VLIB API , i have tried to call the VLIB_integralImage8 function from vlib_c674x_3_3_0_3 VLIB for the souce .cpp file:
VLIB_integralImage8(pIn, (uint16_t)tRect.width, (uint16_t)tRect.height, pLastLine, pOut);//call the API function
while the input variables have been defined correctly accroding to the API guide before i added the call
Meanwhile, i have added the lib library may needed into the c6000 Linker File Search Path as following screenshot shown:
the VLIB_integralImage8.h header file also been added correctly , but after building the project , the error of unresolved symbol VLIB_integralImage8(const, first referenced in unsigned occured everytime?
Note: i have already installed the vlib_c674x_3_3_0_3 into ti directory, and the .lib library shown in the screenshot above was copy from the directoy of C:\ti\vlib_c674x_3_3_0_3\packages\ti\vlib\lib for my project directory, even if i change the c6000 Linker File Search Path into C:\ti\vlib_c674x_3_3_0_3\packages\ti\vlib\lib ,the error still occurs.
Does i have missed some step to compile the VLIB_integralImage8 function API?
Thanks for the assistance.
Best Regards.
laiyi