Other Parts Discussed in Thread: OMAP-L138
Tool/software: Starterware
Hello,
I am working on a 6748 LCDK and have been running programs from chapter 6 of the book "Digital Signal Processing and Applications with the OMAP- L138 eXperimenter." (Specifically Chapter 6 "2 audio IN" adpative filtering) My goal is to run one of these programs from boot loading. All of my program files are working well within the debugger emulation mode, however, when I do the boot loading process, the board will not start the program. Here is the process I have performed:
1. Take the .out file after building the program and use this with the starterware AISgen_d800k008.exe, using the following settings:
2. Set the switches of the LCDK to the proper UART2 Boot mode (off, on, off, on) and connect the USB cable to computer
3. Run the commands on the console to use the starterware program sfh_OMAP-L138.exe in folder C:\ti\pdk_C6748_2_0_0_0\C6748_StarterWare_1_20_03_03\tools\flash_writer using command
sfh_OMAP-L138.exe -targettype C6748_LCDK -flashtype NAND -p COM3 -flash_noubl [bin file name].bin. After this the console says "Operation completed successfully."
4. Swap the bootmode switches to boot from NAND Mode (off, on, on, on) When I listen for the program (its an audio program) the program isn't running.
5. Lastly, I used the debug gel file from the following link to do diagnostics and the gel file reads "Description: C674X_0: Gell Output: Invalid AIS Keyword"
My initial belief is that it has something to do with the program setup, perhaps with the Mcasp peripherals on boot start. Could someone help me figure out what I am doing wrong?? I am currently using CCSv6.
Thanks