Hi,
We are taking an input signal and looping it back to the output.
However, we get a pretty strong noise at the output. Any ideas?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are taking an input signal and looping it back to the output.
However, we get a pretty strong noise at the output. Any ideas?
We are taking an input signal and looping it back to the output.
Exactly. We took the Mcasp audio loopback example.
It uses EDMA, AIC31, Mcasp, RTOS and cache.
That noise is pretty strong, don't you think?
On the LCDK, we connect the input signal to the upper 3.5mm TRS socket, and the output to the lower. What is the maximum voltage the upper socket (the input) can accept?
Hi,
This what happens (the spectrum) when I load a program that generates a constant 39khz wave (ignores the input). The DSP card works on a 96000khz sampling rate:
As you can see, after we load the code, the background becomes darker (blue). That means that there is more noise at the output. Furthermore, before we even load the code, when the background is light blue, there's still too much noise. The only time when there is no background noise is the tiny bright gap that you see in the middle, when the code is loaded. That's the same good noise level that occur when the DSP card is not connected to the sampler (audacity) at all, and that's what we want it be... The noise level is very (very) important to our application, and we can't live with so much noise in the background. We need a clean signal...