The CC in the RX buffer descriptor shows Error, Timeout on receiving one of the segments. This seems to happen occasionally (~20%) at startup between two processors (with a Tundra switch in between). My buffer is 664 bytes long (3 segments). SPRU976E (pg 48) indicates there is a timer involved but does not specify the register and how to set it. Also, it mentions the buffer resources are to be released. How is this done so the RX interrupt is cleared? My application gets stuck continually responding to this interrupt and starves the application of processing time. Thanks.