Tool/software: Starterware
I am currentyl testing Norman's code to write a file to SD card on LCDK C6748.
By adding a delay inside disk_write, I could write a file to SD card but no idea on what cause the code failure without this delay? Can anyone tell me what is the provable reason on this?
Without the delay, I could creat a file but can't write any data into the file, just leaving FR_RW_ERROR message observed on the console.
Furthermore, I want to use Long file name. However, I don't see FATfs R0.04b have any LFN support. Do you happen to have any update on this?
For SDCardPresence Detection, do I just need to set the corresponding pin as input and read the value?
As the last question, if I want to use FAT32, what are the things I need to take care of?