Hello!
My project is design based on ndk 2.0,and DSP c6747. So i try to burn the original ndk 2.0 client example to my spi flash. After compiled correctly, i transformed my .out file to .ais file with the help of AISgen for D800K001. The .ais file has 364 KB. But my program doesn't start because i can't connect the dsp from pc with right ip address.
So please help me ,i want to know whether there are some special steps or configuration to do .
p.s.: I have added the initial functions (setup_system_config, setup_pll, setup_psc_all_on, setup_emifa and setup_emfib) to my main of client.c.
Thank you!