• Resolved

TMS320C6713B: Initial state and direction of GPIO pins after hardware reset

Part Number: TMS320C6713B

HI

HD14 being pulled down  in order to disable HPI and use the GPIO pins, I'm wondering what is the actual (default) state of the gpio pins upon and after a hardware reset.  To me, the C6713 spec seems ambiguious on this.

Thanks

Daniel

U of Sherbrooke

  • Daniel,

    All the pins are tri-stated during POR. The IPU/IPD is activated during POR and its state will be the same during and after reset. You could find the internal pull status in the GPIO terminal functions in data manual.

    Regards,
    Senthil

    ----------------------------------------------------------------------------------------------------------------

    Please click the "Verify Answer" button on this post if it answers your question.