Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
While working with ccs v3.1 on program of sine wave generation following error was generated -
[c6713dskinit.c] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -ppa -fr"C:/CCStudio_v3.1/MyProjects/Debug" -i"C:/CCStudio_v3.1/c6000/dsk6713/include" -d"_DEBUG" -d"CHIP_6713" -mv6710 -@"Debug.lkf" "c6713dskinit.c"
"c6713dskinit.c", line 6: error: identifier "hAIC23_handle" is undefined
"c6713dskinit.c", line 6: error: identifier "config" is undefined
"c6713dskinit.c", line 7: error: identifier "fs" is undefined
"c6713dskinit.c", line 8: error: identifier "DSK6713_AIC23_DATAHANDLE" is undefined
"c6713dskinit.c", line 8: error: identifier "AIC23CfgData" is undefined
"c6713dskinit.c", line 9: error: identifier "MCBSP_XMIT_START" is undefined
"c6713dskinit.c", line 9: error: identifier "MCBSP_RCV_START" is undefined
"c6713dskinit.c", line 10: error: identifier "MCBSP_SRGR_START" is undefined
"c6713dskinit.c", line 10: error: identifier "MCBSP_SRGR_FRAMESYNC" is undefined
"c6713dskinit.c", line 14: error: identifier "poll" is undefined
"c6713dskinit.c", line 19: error: identifier "poll" is undefined
"c6713dskinit.c", line 22: error: identifier "CODECEventId" is undefined
"c6713dskinit.c", line 22: error: identifier "DSK6713_AIC23_codecdatahandle" is undefined
"c6713dskinit.c", line 24: error: identifier "vectors" is undefined
"c6713dskinit.c", line 32: error: declaration is incompatible with previous "output_sample" (declared at line 30)
"c6713dskinit.c", line 35: error: identifier "AIC_data" is undefined
"c6713dskinit.c", line 38: error: identifier "poll" is undefined
"c6713dskinit.c", line 38: error: identifier "DSK6713_AIC23_DATAHANDLE" is undefined
"c6713dskinit.c", line 44: error: identifier "poll" is undefined
"c6713dskinit.c", line 44: error: identifier "DSK6713_AIC23_DATAHANDLE" is undefined
"c6713dskinit.c", line 45: error: identifier "AIC_data" is undefined
"c6713dskinit.c", line 46: error: identifier "LEFT" is undefined
"c6713dskinit.c", line 51: warning: variable "poll" was declared but never referenced
22 errors detected in the compilation of "c6713dskinit.c".
>> Compilation failure
[sine8_LED.c] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -ppa -fr"C:/CCStudio_v3.1/MyProjects/Debug" -i"C:/CCStudio_v3.1/c6000/dsk6713/include" -d"_DEBUG" -d"CHIP_6713" -mv6710 -@"../Debug.lkf" "sine8_LED.c"
"sine8_LED.c", line 1: fatal error: could not open source file "c6713dskinit.c"
1 fatal error detected in the compilation of "sine8_LED.c".
Compilation terminated.
>> Compilation failure
[vectors_poll.asm] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -ppa -fr"C:/CCStudio_v3.1/MyProjects/Debug" -i"C:/CCStudio_v3.1/c6000/dsk6713/include" -d"_DEBUG" -d"CHIP_6713" -mv6710 -@"Debug.lkf" "vectors_poll.asm"
"vectors_poll.asm", ERROR! : [E0000] Can't find end of 'VEC_ENTRY' macro
definition starting on line 19 --
Aborting!
>> Compilation failure
Build Complete,
24 Errors, 1 Warnings, 0 Remarks.
How to get rid of it???