Greetings everybody!
I am Akshay. I am trying to use the boards that are avail be in the DSP lab. These are the ones from 2005. The DSP boards number I am trying to connect is TMDSDSK6713. As the lab hasn't been used for a while i don't have access to any of the prerequisite files. If somebody can help me with that it would great. I am using Matlab 2015a and CCSv5.1.1 does board work on these platforms or do I have to use the older versions.?