Other Parts Discussed in Thread: OMAPL138
Hi
I have created a new project in CCS with the following simple program:
int main(void) { int i; int j = 0; for(i = 0; i < 1000000; i++) { j++; } return 0; }
After some time the program hangs (it seems to be at a random point) and when the debugger is suspended then it shows:
No source available for "0xc3d38e84"
But this address is DDR2, while the linker command file specifies Shared RAM. The main function has address 0x80000ee0, which is in Shared RAM, as expected. I have used an existing RTSC successfully, but I want to have a CCS project.
What is going on? Am I forgetting something?
I am using the following hardware and software:
TMDSLCKD6748
XDS100v2 JTAG 14-pins
CCS Version: 7.2.0.00013
I have attached the CCS project-files.1222.TryDspL2RAM.zip
Best regards
Ad