Hi,
I want to connect external sdram on CE0 of tms320c6713 in 16-bit mode. From spru266e, c6713 read/write in 4-word bust mode. As the interface is 16-bits thus the total bits read/written will be 64bits (16×4).
My question is how the C program can be written to read/write 64 bits at a time?? Will it look like this:
uint64_t *sdram = (uint64_t *)0x80000000
//write acceas 64 bits
*sdram = 0x1234567812345678
//read access
Uint64_t xyz = *sdram
Kindly correct me, as this code doesnt work.
Kind regards,