Hi, I am using the TMDSLCDK138 for my application. So far, I managed to transfer samples from the codec to the external memory using EDMA3 and McASP and then send them back to the codec without doing any processing.
I would like to apply a symmetric FIR filter to the samples and for that I had a look at DSPLIB. Especifically, I downloaded the package dsplib_c674x_3_4_0_0.
While it has a function for generic FIR filtering, there is no function for applying a symmetrical FIR. Why? I have thought that perhaps the reason is related with the architecture and there is no advantage in using this type of FIR implementation.
I am not using any SO or anything, it's all code from scratch, but I would like to optimize the DSP operations.
Sorry if this is not the appropiate forum and thanks in advance.