Tool/software: TI-RTOS
Hello!
I got a problem with UART_BasicExample_lcdkOMAPL138_c674xExampleProject and others examples that uses UART.
I installed SDK and built example without errors using CCS 7.3.
Before run the example I’ve extracted sd-card from the LCDKOMAPL138 board, so I expect that u-boot powers up DSP-core and Linux doesn’t work and use any resources.
Then I connected Terminal to the board and after power up the first characters in the terminal is the u-boot output. Then I started example application using CCS and USB510L JTAG Emulator.
When application preform code
UART_puts("\nuart driver and utils example test cases :\nEnter 16 characters or press Esc \n",sizeof("uart driver and utils example test cases : please enter 16 characters or press Esc or carriage return\n"));
... I see unreadable symbols in terminal.
Then when application go through code line
UART_gets(buffPointer, INPUT_LENGTH);
... it blocks and it doesn’t unblocks even I type a lot of characters in terminal.
Can you explain me why it’s going wrong?