Tool/software: Code Composer Studio
I have several TMS320C6713B boards that I'm currently trying to program, but about half of them refuse to connect to CCS or the 6713 DSK Diagnostics Utility.
The boards that connect all report a USB ID of 0C55:6713, while the ones that I can't connect to all report 0451:9000.
Note that is has no correlation to whether or not the board actually works - these boards had previously been programmed with an earlier version of the software and deployed to the field, and all of their internal software diagnostics still pass just fine regardless of whether I'm able to connect to them.
However, in order to update the software version I need to be able to connect to them with CCS to run the firmware patch program. Of all the ones I'm able to connect to (those with ID 0C55:6713), I haven't had any issues, but I can't program any of the ID 0451:9000 ones at all.
It's unclear whether this is just an issue with the software not recognizing the devices, or if there is a deeper problem with the USB interface.
How can I fix this issue so I can program the other boards?
I'm currently running CCS 3.1.0 I've tried to find other newer versions, but I can't get any of them to work even with the 0C55:6713 boards so for