Tool/software: Code Composer Studio
I was using one of the programs from Chassaing textbook where we use one board as the transmitter and the other board as a receiver using BPSK modulation. When i build both the programs the .out file is successfully generated without any errors. But, when i give an input to the transmitter i don't get to hear anything at the receiver. Can somebody figure out why this is happening/
I also tried to build a Simulink model to do the same. That also goes through the building process but when i try to give an input there is no output. I can attach the Simulink model if you guys want to have a look at it.
Is it something wrong with respect to the board as i don't think it is something wrong with the board as it worked for a lot of other examples.
Attached are the .c files of the transmitter and the receiver.
transmitter.c
//transmitter.c Transmits voice as a BPSK signal
#include "dsk6713_aic23.h" //codec-DSK support file
#include <math.h>
#include "lp1500.cof" //1500 Hz coeff lowpass filter
Uint32 fs=DSK6713_AIC23_FREQ_48KHZ; //set sampling rate
#define DSK6713_AIC23_INPUT_MIC 0x0015
#define DSK6713_AIC23_INPUT_LINE 0x0011
Uint16 inputsource=DSK6713_AIC23_INPUT_MIC;//select input
#define NUMSAMP 4 //# samples per Symbol
#define MAX_DATA_LENGTH 10 //size of Mod/Demod vector
#define NUM_BITS 8 //number of bits per sample
#define SYNC_INTERVAL 100 //interval between sync bits
short encSeqNum = 8; //number of encoded bits
short encSymbolVal = 0; //encoder symbol index
short sin_table[NUMSAMP]={0,1000,0,-1000}; //for carrier
short bits[8]; //holds encoded sample
short sampleBuffer[2000]; //to view sample
short sIndex = 0; //index sampleBuffer
short syncSequence[8]={1,1,1,-1,1,-1,-1,1}; //syncronization sequence
short outval=1; //bit value to be encoded
short encodeVal = 0; //filtered input value
int yn = 0; //init filter's output
short gain=10; //gain on output
short syncTimer = 0; //tracks time between syncs
#define LEFT 0 //setup left/right channel
#define RIGHT 1
union {Uint32 uint; short channel[2];} AIC23_data;
interrupt void c_int11() //interrupt service routine
{
int i;
short sample_data;
sample_data = input_sample();
yn = fircircfunc(sample_data,h,N); //asm func passing to A4,B4,A6
if(encSymbolVal >= NUMSAMP) //increment through waveform
{
encSymbolVal = 0;
encSeqNum++;
}
if(encSeqNum == NUM_BITS) //when all 8 bits sent
{ //get a new sample
encSeqNum = 0;
if(syncTimer++ >= SYNC_INTERVAL) //determine whether
{ //to send sync sequence
syncTimer = 0;
for(i=0; i<8; i++) //put sync sequence in bit
bits[i] = syncSequence[i];
}
else
{ //get the bits
encodeVal = (short) (yn >> 15);
for(i=8; i<16; i++) //encode input sequence
bits[i-8]=(encodeVal & (1<<i)) ? 1 : -1; //shift
}
sampleBuffer[sIndex++] = encodeVal;
if(sIndex >= 2000) sIndex = 0;
}
outval = (short) bits[encSeqNum];
AIC23_data.channel[RIGHT]=gain*sin_table[encSymbolVal];//carrier->Right Channel
AIC23_data.channel[LEFT]=gain*outval*sin_table[encSymbolVal++];//data->Left
output_sample(AIC23_data.uint); //output to both channels
}
void main(){
comm_intr();
while(1); } //init,infinite loop
recevier.c
//Receiver.c Demodulates received BPSK voice signal
#include "dsk6713_aic23.h" //codec-DSK support file
#include <math.h>
Uint32 fs=DSK6713_AIC23_FREQ_96KHZ; //set sampling rate
#define DSK6713_AIC23_INPUT_MIC 0x0015
#define DSK6713_AIC23_INPUT_LINE 0x0011
Uint16 inputsource=DSK6713_AIC23_INPUT_MIC;//select input
#define NUMSAMP 8 // # Samples per Symbol
#define NUM_BITS 100
#define PI 3.1415926
#define SYNC_INTERVAL 100 // Interval between sync sequence
short carrier_sample; // input sample
short data_sample;
short carrier_symbol[NUMSAMP]; // buffer to received one period of carrier
short data_symbol[NUMSAMP*2]; // buffer to received one period of data
short csIndex=0; // symbol buffer index
short dsIndex=NUMSAMP; // symbol buffer index
short phIndex=0;
#define NPHI 100
float phiBuf[NPHI]={0}; // buffer to view phi estimates from PLL
short phiBind=0; // phi buffer index
short phiLoop = 0; // Used to determine if Phi looped beyond 0<phi<2PI
float sin_table[96*NUMSAMP]; // a table of 3 periods of a sin wave
short pow_table[16]; // a table of powers of two
float y1, y2; // correlation vectors
float phi=PI; // phase estimate
float dphi = 0; // change in phi
float damp=1; // damping factor
short decSeqNum = 0; // Number of encoded bits
short decodeSeq[9]={0}; // Encoder Symbol Index
short syncSequence[8] = {1,1,1,0,1,0,0,1}; // Syncronization Sequence
short syncTrigger = 0; // Trigger to determine if Sync Seq is found
short syncInterval = 0; // Looks for the interval between Sync Seqs
short rBit[2]; // Received bits
short bits[8]={0}; // Received bits in one frame
short bitIndex=0; // Index into frame
short nrBits = 0; // Determines how many received bits are in buffer
short out_sample = 0; // current received sample
short prev_sample = 0; // previously received sample
short prev_sample2 = 0; // received two sample before current sample
short outInc = 0; // Increments through the interpolation polynomial
// DEBUG VARIABLES
short TrigBuffer[200] = {0}; // Used to look at incoming trigger values
short tbIndex = 0; // Index into TrigBuffer
short carrierBuffer[1000]; // Buffer for the carrier wave
short dataBuffer[1000]; // Buffer for the BPSK Data wave
short bufIndex = 0; // Index into carrierBuffer & dataBuffer
short sampleBuffer[2000]; // Buffer of output Samples
short sBuffer = 0; // Index into sampleBuffer
int X=0; // Used in correlation receiver
interrupt void c_int11() //interrupt service routine
{
int i,j;
int max=1;
carrier_sample = (short) input_right_sample(); //receive carrier
data_sample = (short) input_left_sample(); // receive data
carrier_symbol[csIndex++] = carrier_sample; // put carrier in symbol buffer
data_symbol[dsIndex++] = data_sample; // put data in symbol buffer
carrierBuffer[bufIndex] = carrier_sample; // debug carrier values
dataBuffer[bufIndex] = data_sample; // debug data values
if(++bufIndex >= 1000)
bufIndex = 0;
if(csIndex >= NUMSAMP) // after one period is received
{ // then perform phi estimate
y1 = 0;
y2 = 0;
csIndex = 0; // Reset Index
dsIndex = NUMSAMP;
for(i=0; i<NUMSAMP; i++) // correlate received carrier symbol
{
y1 += carrier_symbol[i]*sin_table[32*(NUMSAMP + i + phIndex) - 1];
y2 += carrier_symbol[i]*sin_table[32*(NUMSAMP + i + phIndex) + 1];
if(carrier_symbol[i] > max)
max = carrier_symbol[i];
}
if(max != 0)
{
y1 = y1 / max; // normalize correlation coefs
y2 = y2 / max;
}
else
{
max = 1;
}
dphi = 0.2*(y2 - y1); // Calculate derivative to find the maximum
// of the matched filter
if(dphi > PI) // help keep phi within 0<phi<2*PI
dphi = PI;
phi = phi + dphi; // determine new estimate for phi
phiLoop = 0;
if(phi < 0) // normalize phi to 0<phi<2*PI
{
phi = phi + 2*PI;
phiLoop = -1;
}
if(phi > (2*PI))
{
phi = phi - 2*PI;
phiLoop = 1;
}
phiBuf[phiBind++]=phi; // put phi in buffer for viewing
if(phiBind >= NPHI) // resent buffer index
phiBind = 0;
phIndex = (int) (NUMSAMP-1)*phi/(2*PI); // update phi's index into correlators
if(phiLoop == 0) // No wrapping
{ // Receive one bit
X = 0;
for(i=0; i<NUMSAMP; i++) // Correlate Signal with Basis Function
{
X += data_symbol[(NUMSAMP-1)-phIndex+i]*sin_table[32*i];
data_symbol[i] = data_symbol[NUMSAMP + i];
}
rBit[0] = (X >= 0) ? 1: 0; // Make Detection
nrBits = 1;
}
if(phiLoop == 1) // phi wrapped to 0
{ // Received two bits
phiLoop = 0;
X = 0;
for(i=0; i<NUMSAMP; i++) // Correlate Signal with Basis Function
{
X += data_symbol[i]*sin_table[32*i];
}
rBit[0] = (X >= 0) ? 1: 0; // Make Detection;
X = 0;
for(i=0; i<NUMSAMP; i++) // Correlate Signal with Basis Function
{
X += data_symbol[(NUMSAMP-1)-phIndex+i]*sin_table[32*i];
data_symbol[i] = data_symbol[NUMSAMP + i];
}
rBit[1] = (X >= 0) ? 1: 0; // Make Detection
nrBits = 2;
}
if(phiLoop == -1) // Phi wrapped to 2*PI
{ // don't receive any bits
phiLoop = 0;
for(i=0; i<NUMSAMP; i++)
{ // update symbol values
data_symbol[i] = data_symbol[NUMSAMP + i];
}
nrBits = 0;
}
for(i=0; i<nrBits; i++) // Loop over the received bits
{
bits[bitIndex++] = rBit[i];
decodeSeq[7] = rBit[i]; // put received bit in decSeq Buffer
syncTrigger = 0;
for(j=0; j<8; j++) // Search the last 8 bits for
{ // frame syncronization sequence
if(j < 8) // mask received seq with sync seq
{
syncTrigger += (decodeSeq[j] == syncSequence[j]);
}
decodeSeq[j] = decodeSeq[j+1];
}
syncInterval++;
if(syncTrigger == 8) // If sync interval is found set frame index
{
if(syncInterval == 8*(SYNC_INTERVAL+1)) // Look for symbols separated
{ // by the sync interval
bitIndex = 0; // Set the frame sync point
prev_sample2 = prev_sample; // Use same values
prev_sample = out_sample; // for output if sync bit is present
}
syncInterval = 0;
}
TrigBuffer[tbIndex++] = syncTrigger; // Debug buffer to look at trig
if(tbIndex >= 200) // Reset trig buffer index
tbIndex = 0;
if(bitIndex >= 8) // If a byte is received decode it
{
prev_sample2 = prev_sample; // Update 3rd polynomial vertex
prev_sample = out_sample; // Update 2nd polynomial vertex
bitIndex = 0; // reset index into bit buffer
out_sample=0; // set output sample to zero
outInc = 0; // Reset polynomial interp index
if(bits[7]==1) // If negative value take twos comliment
{
for(j=0;j<7;j++) // Mask bits twos compliment
{
bits[j] = (bits[j] == 0);
}
}
for(j=8; j<15; j++) // Decode the bits
{
out_sample=out_sample+pow_table[j]*bits[j-8];
}
if (bits[7]==1) // If negative change the sign and add 1*2^8
{
out_sample=-(out_sample+256);
}
sampleBuffer[sBuffer++] = out_sample;
if(sBuffer >= 2000)
sBuffer = 0;
}
}
if(decSeqNum >= NUM_BITS) // Reset index for decoded sequence
{
decSeqNum = 0;
}
}
// Use 3 point polynomial interpolation for output values
output_sample((out_sample-2*prev_sample + prev_sample2)*(outInc*outInc/64-outInc)/128
+ (prev_sample-prev_sample2)*outInc/64 + prev_sample2);
outInc++;
}
void init_sin_table() // Tables used to speed computation
{
int i;
for(i=0; i<96*NUMSAMP; i++) // Create table of sin waves
{
sin_table[i] = sin(2*PI*i/(32*NUMSAMP));
}
for(i=0; i<16; i++) // Create Table of powers of two
{
pow_table[i] = pow(2, i);
}
}
void main()
{
init_sin_table();
comm_intr(); //init DSK, codec, McBSP
while(1); //infinite loop
}