I'm looking for examples of code for the USB port on the C6748.
I've found the TMS320C674x/OMAP-L1x Processor Universal Serial Bus 2.0 (USB2.0) Controller (sprufm9h.pdf). And I've found the raw specification for the USB 2.0 standard. And I've found some sample test code that comes with the LogicPD C6748 EVM board. Nonetheless it's still looking like a huge research project, since USB is more complicated than most peripherals.
I need code that will allow a Host PC to occasionally send numeric values over the USB into specific memory locations of the DSP -- and perhaps to read them back again. That's pretty simple as USB applications go.
Any tips or hints would be appreciated.