Hi,
I'm sending from an FPGA thirteen 32 bits words every 25us on the mcasp_rx[0] pin of my DSP running at 50Mhz. There are 32 spare clock cycles after every word.
The McASP is configured as follow : (burst mode, 32bits, NO_DMAX defined...)
void McASP0_start( void ) { unsigned i,gblctl_temp; GBLCTL_0= 0x00000000; while(GBLCTL_0!=0x00000000); PWRDEMU_0= 0x00000001; RMASK_0= 0xFFFFFFFF; #ifdef NO_DMAX RFMT_0= 0x000000F8; #else RFMT_0= 0x000000F0; #endif AFSRCTL_0= 0x00000000; ACLKRCTL_0= 0x00000000; AHCLKRCTL_0= 0x00000000; RTDM_0= 0x00000001; RINTCTL_0= 0x00000000; XMASK_0= 0xFFFFFFFF; XFMT_0= 0x000000F8; AFSXCTL_0= 0x00000002; ACLKXCTL_0= 0x000000C0; AHCLKXCTL_0= 0x00000000; XTDM_0= 0x00000001; XINTCTL_0= 0x00000000; for(i=0;i<NB_SERIALIZER_MCASP0;i++) { SRCTL_0(i)= 0x00000000; } SRCTL_0(0)= 0x00000002; SRCTL_0(1)= 0x00000001; PFUNC_0= 0x4A00FFF0; PDIR_0= 0x1000000A; DITCTL_0= 0x00000000; DLBCTL_0= 0x00000000; AMUTE_0= 0x00000000; GBLCTL_0= 0x00000202; while(GBLCTL_0!=0x00000202); #ifndef NO_DMAX DMAX_mcasp0_start_fifo(); #endif XSTAT_0= 0x0000FFFF; RSTAT_0= 0x0000FFFF; gblctl_temp=GBLCTL_0|GLBCTL_RSRCLR|GLBCTL_XSRCLR; GBLCTL_0=gblctl_temp; while(GBLCTL_0!=gblctl_temp); gblctl_temp=GBLCTL_0|GLBCTL_RSMRST|GLBCTL_XSMRST; GBLCTL_0=gblctl_temp; while(GBLCTL_0!=gblctl_temp); gblctl_temp=GBLCTL_0|GLBCTL_RFRST|GLBCTL_XFRST; GBLCTL_0=gblctl_temp; while(GBLCTL_0!=gblctl_temp); }
If I read the received values from RBUF_0, every thing is fine, all data are received as expected. The McASP is then well configured for my application !!!
I now use the DMAX to read automatically the datas in a fifo.
The DMAX is configured as follow (NO_DMAX is undefined now):
#define DMAX_FIFO_SIZE 130 #define DMAX_FRAME_SIZE 13 unsigned Dmax_fifo_descriptor_mcasp0[7], Dmax_fifo_buffer_mcasp0[DMAX_FIFO_SIZE]; void DMAX_mcasp0_start_fifo (void) { unsigned i; Dmax_mcasp0_number_of_restart_counter++; for(i=0;i<DMAX_FIFO_SIZE;i++) { Dmax_fifo_buffer_mcasp0[i]=0xDEADBEEF; } DEDR= 0x00000020; LOMAX_EVENT_05_ENTRY_MCASP0_RX= 0x01112804; LOMAX_TRANSFER_00_ENTRY_00= MCASP0_DMA_PORT_ADDR; LOMAX_TRANSFER_00_ENTRY_01= ((unsigned)Dmax_fifo_descriptor_mcasp0); LOMAX_TRANSFER_00_ENTRY_02= 0x00000001; LOMAX_TRANSFER_00_ENTRY_03= 0x00000001; LOMAX_TRANSFER_00_ENTRY_04= 0x00000000; LOMAX_TRANSFER_00_ENTRY_05= 0x00000001; LOMAX_TRANSFER_00_ENTRY_06= MCASP0_DMA_PORT_ADDR; LOMAX_TRANSFER_00_ENTRY_07= MCASP0_DMA_PORT_ADDR; LOMAX_TRANSFER_00_ENTRY_08= 0x00000000; LOMAX_TRANSFER_00_ENTRY_09= 0x00000000; LOMAX_TRANSFER_00_ENTRY_10= 0x00000000; Dmax_fifo_descriptor_mcasp0[0]= ((unsigned)Dmax_fifo_buffer_mcasp0); Dmax_fifo_descriptor_mcasp0[1]= 0x00000000; Dmax_fifo_descriptor_mcasp0[2]= (0x2<<24) + DMAX_FIFO_SIZE; Dmax_fifo_descriptor_mcasp0[3]= 0x00000000; Dmax_fifo_descriptor_mcasp0[4]= DMAX_FRAME_SIZE; // edit: remove -1, but it doesn't solve the problem Dmax_fifo_descriptor_mcasp0[5]= 0x01000000; Dmax_fifo_descriptor_mcasp0[6]= 0x00000000; DELPR= 0x00000020; DEPR |= 0x00000020; DFSR0= 0x00000003; DTCR0= 0x00000002; DEFR= 0x00000020; DEER= 0x00000020; }
As I understand, DMAX is configured to send an interrupt every thirteen 32 bits received words on the McASP. Datas are written automatically in fifo.
In the interrupt 7 function, I read the 13 last received data from the fifo, but once in a while data[9] or data[10] is 1 bit right rotated.
I don't understand why. Can someone have an explanation for this behavior and a workaround ?
thanks
Aurélien