Hello!
I can't connect to some of my custom TMS320C6713BGDP-boards. The diagnostics in the SDConfig-Tool works, but when I try to connect to the board using CCS 3.3 the following error-message appears:
------------------- begin ------------------------
Error connecting to the target:
Error 0x80000202/-1060
Fatal Error during: Memory, OCS,
An unknown error prevented the emulator from accessing the processor
in a timely fashion.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
I/O Port = 510
Board Name: Memfis
Cpu Name: cpu_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
------------------- end ------------------------
The V-core seems to be stable (tested with some osci).
Any idea, what else I can check. Unfortunatly its hard to check for shorts on a ballgrid.
Best regards,
Thomas