• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » C6000 Single Core DSP » C67x Single Core DSP Forum » All Tags » 6747
Share
C6000 Single Core DSP
  • Forums
  • Announcements

Browse by Tags

C6000 Single Core DSP

Welcome to the C6000 Single Core DSP Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
6747
  • 6713
  • 6713 DSK
  • 672x
  • 6748
  • 674x
  • 67XX
  • boot
  • bootloader
  • C6000
  • C6713
  • C6713B
  • C6747
  • C6748
  • C674x
  • C67x
  • CCS v3.3
  • DSK6713
  • dsp
  • DSP/BIOS
  • EMIF
  • HPI
  • interrupts
  • McASP
  • SPI
  • tms320c6713
Related Posts
  • Forum Post: Re: Reconfiguring Audio and McASP drivers for custom hardware

    David Anderson11625 David Anderson11625
    Hi there, thank you all for the detailed and informative replies. By the end of Friday I had figured out that the parameter "bios.UDEV.instance("mcasp0").deviceId" referred to the number of the physical McASP to be used in that driver. I put a big old comment in the code to that...
    on May 18, 2009
  • Forum Post: BIOSUSB

    Ana Leticia Ana Leticia
    Hi, Could anyone used BIOSUSB? I´m trying to use it with my board (without SDRAM). So the examples can not be used because the code is too large and not can be allocated on the internal RAM. I need to make a simple USB PC / board communication (HID is ok for me). Does anyone be successfull writing...
    on Aug 26, 2009
  • Forum Post: burn FPGA program to flash and loard the dsp program to sdram

    yunpeng ma yunpeng ma
    Hi, i have two questions. 1. I am using tms320c6747 ,now i want to burn the fpga program(bit file) to the flash ,then read the fpga program to fpga and make it run in fpga, but i do not know how to burn the bit file to the flash, so thanks for telling me to do this. 2. my dsp program is too big...
    on Mar 3, 2010
  • Forum Post: Re: burn FPGA program to flash and loard the dsp program to sdram

    yunpeng ma yunpeng ma
    Thanks for your answer , can you tell me how to transform the fpga bit file to ais or bin file. do you have such tools to do this . thanks!
    on Mar 4, 2010
  • Forum Post: Re: how to loard the rts67plus.lib correctly and the differences between rts67plus.lib and rts6740.lib

    yunpeng ma yunpeng ma
    Mariana yunpeng ma 1.in the cmd file,when i write '-l rts67plus.lib' and select -mv674x in build options.there will be a link error (undefined symbols , first reffered).but when i select -mv6700 in build options,there is no error at all. Make sure that you have CGT 6.1.9 or later: http...
    on Mar 10, 2010
  • Forum Post: Re: how to loard the rts67plus.lib correctly and the differences between rts67plus.lib and rts6740.lib

    yunpeng ma yunpeng ma
    Mariana yunpeng ma 1.in the cmd file,when i write '-l rts67plus.lib' and select -mv674x in build options.there will be a link error (undefined symbols , first reffered).but when i select -mv6700 in build options,there is no error at all. Make sure that you have CGT 6.1.9 or later: http...
    on Mar 10, 2010
  • Forum Post: how to loard the rts67plus.lib correctly and the differences between rts67plus.lib and rts6740.lib

    yunpeng ma yunpeng ma
    Hi, I am using tms3206747 ,now i have two questions. 1.in the cmd file,when i write '-l rts67plus.lib' and select -mv674x in build options.there will be a link error (undefined symbols , first reffered).but when i select -mv6700 in build options,there is no error at all. 2.i don't...
    on Mar 9, 2010
  • Forum Post: Is AISGen for D800K003 compatible with D800K001 if I do not use the new commands?

    Mark Rae Mark Rae
    I am doing some initial development on the EVM 'C6747 that uses the D800K001 bootloader. Our custom target is a TMS320C6745B which uses D800K003. I will be booting from the SPI Flash on both platforms. If I do not use the new commands like configuring the pin mux can I run the boot file created...
    on Jun 3, 2010
  • Forum Post: Multiple UART interfaces

    Uri Shkolnik Uri Shkolnik
    Hi, [[ Env.: C6748 DSP, CCS4, PSP 1.30.1 ]] I'm trying to initialize and use multiple UARTs interfaces simultaneously. UART2 works "out of the box" (using the example given within the PSP) I couldn't find a way to initialize and use UART0 and UART1 (all UART work at...
    on Jun 3, 2010
  • Forum Post: DSPlib function DSPF_sp_biquad not working with non-whole number coefficients

    Arvid Tomayko-Peters Arvid Tomayko-Peters
    Hi I'm trying to use the DSPlib's single precision biquad function on a C6747 EVM. The problem is that when I give it coefficients that are not whole numbers, I get awful noise out, even with no audio input (though the noise changes when there is audio input). But when I use coefs that...
    on Jun 10, 2010
  • Forum Post: Re: Select Device

    June He June He
    Dear Daniel Thanks for you suggestion, I have looked up in TI's website, and also have looked at the datsheet about TMS320C6745/6747 , However , no QFP [PYP suffix] were be founded, just only BGA [ ZKB suffix] package for TMS320C6747, and 6748 too. Are you sure that the 6747 include QFP(Quad...
    on Jul 3, 2010
  • Forum Post: Re: Select Device

    June He June He
    Yes, 256M of SDRAM space is enough, but more than two 16-bit EMIF interface are asked for FPGA and FLASH Another question is confused me : as you say , the 6745/6743 include 16-bit interface ,Are the 32-bit instruction can run in a 16-bit width SDRAM ? the 32-bit variable can be accessed or storaged...
    on Jul 3, 2010
  • Forum Post: Re: Programming the DSP

    caleb crome caleb crome
    I set up my board with external circuitry (controlled by an MSP430 that we needed anyway), so that it can boot from NOR flash, UART2, or EMULATION mode. This is done by configuring the BOOTx pins with configurable pullup or pulldown resistors. The bootloader documentation tells which pins do what. To...
    on Jul 21, 2010
  • Forum Post: How to burn ndk 2.0 to spi flash

    huichao zhou huichao zhou
    Hello! My project is design based on ndk 2.0,and DSP c6747. So i try to burn the original ndk 2.0 client example to my spi flash. After compiled correctly, i transformed my .out file to .ais file with the help of AISgen for D800K001. The .ais file has 364 KB. But my program doesn't start because...
    on Aug 1, 2010
  • Forum Post: edma3 AXEVT signal not being generated from MCASP module

    caleb crome caleb crome
    Hello, I'm using our custom C6745 board, trying to bring up EDMA with the McASP, without using the BSP. The BSP footprint is simply too large (we don't have any external RAM), and when I compiled the BSP DMA and McBSP drivers in, they were something like 150k combined. Anyway, I'm using...
    on Jul 21, 2010
  • Forum Post: How to see the value of a register

    huichao zhou huichao zhou
    I use the EDMA of 6747 in my project.After setup of the register OPT of EDMA, i input the address of register OPT in the window of "memory" in order to see the value i send to it, but the value in memory is not what i send and seems not change. In my opinion , the register is a part of memory...
    on Jan 10, 2011
  • Forum Post: HPI interface doesn't work after HPI boot

    Daniele Vismara Daniele Vismara
    Hi, we are working with a system with a ColdFire processor that work as host and two DSP TMS320C6747 connected as slave with HPI interface. Using bootloader to perform boot via HPI, we have a problem: after launch of program with DSPINT assertion, according to bootloader procedure, the program...
    on Feb 28, 2011
  • Forum Post: Re: Distortion in Audio with McASP using EDMA3 - Low level Coding

    sudheer thota sudheer thota
    IS there any one can help me EDMA3 setting?
    on Mar 9, 2011
  • Forum Post: ndk project output "no phy connected"

    huichao zhou huichao zhou
    I use the ndk on C6747, my net drive chip is dm9161.But when i run my project ,it output "no phy connected". I have checked my net chip, there are no signal on the port of MDIO and MDC. Is the layout of MAC broken or some errors else? Thank you!
    on Apr 10, 2011
  • Forum Post: DDR2 Initialization (GEL)

    Uri Shkolnik Uri Shkolnik
    Hi, I'm straggling with the initialization of DDR2 ( Micron MT47H32M16, 8 Meg x 16 x 4 banks ). My environment is C6748 @ 300MHz, the DDR2 is 400MHz capable, and so I'm trying to configure the DSP DDR controller to 150MHz (the controller's maximum). There are multiple problems…...
    on Jun 21, 2010
  • Forum Post: Re: timer

    Ricardo Zepeda Ricardo Zepeda
    If you notice TIMER_EVENT0, TIMER_EVENT1, TIMER_EVENT2 and TIMER_EVENT3 are used by the CSL_FINS function. The declaration of the CSL_FINS function is as follows…. CSL_FINS(reg, field, val). In essence they are placing values 04, 64, 40 and 48 to intcRegs->INTMUX1 register. The C6747...
    on Aug 10, 2011
  • Forum Post: events

    Leandro Souza Leandro Souza
    good day Someone could help me figure out why the example below , #define GPIO0_EVENT 65 must be 65 if I change the value to 66 for example does not work because that is what has to be 65 . thanks /* sys config registers overlay */ CSL_SyscfgRegsOvly sysRegs = (CSL_SyscfgRegsOvly...
    on Aug 12, 2011
  • Forum Post: TIMER

    Leandro Souza Leandro Souza
    good day I'm more a doubt using cslr how do I read the contents of the timer that is I put the timer to tell and want to make a comparison in metado count then I wanted to know how to read the contents of the timer. Obribado .
    on Aug 8, 2011
  • Forum Post: Configuração do timer

    Leandro Souza Leandro Souza
    Good day I'm trying to make a program that when the code enters a loop it enables the led there a timer that counts a time and then disable the timer turns off the LED timer enables the new account a while back and disable the timer to the beginning and is well but I can not set the timer to...
    on Aug 8, 2011
  • Forum Post: Mcasp

    Leandro Souza Leandro Souza
    good day Look, I 'm looking at an example that follows encontra c: ->arquivo de programas-> texas intrument-> pspdrivers_01_20_00->packages-> ti->pspiom->examples-. evm6747->audio. of a screen. I wonder because when I debug it step by step F11 tight when he arrives...
    on Aug 24, 2011
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use