• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » C6000 Single Core DSP » All Tags » C6000
Share
C6000 Single Core DSP
  • Forums
  • Announcements

Browse by Tags

C6000 Single Core DSP

Welcome to the C6000 Single Core DSP Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
C6000
  • 6455
  • 6713
  • 6713 DSK
  • 672x
  • 6747
  • 6748
  • 674x
  • 67XX
  • bios
  • boot
  • boot mode
  • bootloader
  • c++
  • C64+
  • c6416
  • C6424
  • C6455
  • C6457
  • C64x
  • C64x+
  • C6713
  • C6713 DSK
  • C6713B
  • C6713DSK
  • C6727
Related Posts
  • Forum Post: Re: Changing Registers

    TimHarron TimHarron
    The C6000 architecture can be difficult to follow if not familiar with it. The optimizer takes your code and packs it together as tightly as possible. This can cause confusing behavior as some instructions have inherent delay slots before execution finishes. For example, the LDW has 4 delay slots before...
    on Jul 16, 2008
  • Forum Post: Re: Changing Registers

    jyoung jyoung
    Tim, Thanks for the reply. We may have found our problem. When we read a double out of SDRAM the value is corrupted. When looking at memory the lower 32 bits are correct but the upper 32 are duplicates of bits 15-8. We are investigating this. Jim
    on Jul 16, 2008
  • Forum Post: how to do 64-bit word norm operation?

    Xuedong Xuedong
    Anyone knows how to do 64-bit word norm operation? From TMS320C6000 programmer's guide, I can find uint _norm(int src2) for 32-bit word uint _lnorm(long src2) for 40-bit word intrinsics. But there is no norm intrinsic is defined for 64-bit word. Thanks.
    on Sep 2, 2008
  • Forum Post: How to do a multiplication of two 32-bit words?

    Xuedong Xuedong
    Anyone knows how to do a multiplication of two 32-bit words in C? From TMS320C6000 programmer's guide, I can find _mpyhi() and _mpyli() intrinsics for 16bit and 32bit multiplicaiton. But there is no intrinsic is defined for a multiplication of two 32-bit words. Thanks.
    on Sep 2, 2008
  • Forum Post: Re: How to do a multiplication of two 32-bit words?

    TimHarron TimHarron
    This depends on which processor you are using. The C6412 and C6416 for example do not have such intrinsics; however, C64x+ and C674x+ parts have several intrinsics for 32x32 multiplication ( _mpy32ll, _mpy32su, _mpy32us, _mpy32u). See pages 169-173 of the C6000 Optimizing Compiler User's Guide linked...
    on Sep 3, 2008
  • Forum Post: Re: how to do 64-bit word norm operation?

    TimHarron TimHarron
    The _lnorm and _norm intrinsics are the only two I know of for all C6000 parts. See pages 169-173 of the C6000 Optimizing Compiler User Guide (spru187o). http://focus.ti.com/lit/ug/spru187o/spru187o.pdf
    on Sep 3, 2008
  • Forum Post: How to measure the cycles of a function multiple times automatically in the simulator?

    Xuedong Xuedong
    Hi, I have a question: how to measure the cycles of a function multiple times automatically in the simulator? More specific, I have the following C file main function and want to measure the cycles of the function xyz() inside the for loop 100 times and save the cycles somewhere. So I can analyze...
    on Nov 6, 2008
  • Forum Post: Re: TMS320C6000 HPI

    BrandonAzbell BrandonAzbell
    Camila Nunes The device is TMS320C6202 DMA. A document I would suggest using is the TMS320C620x/C670x DSP Program & Data Memory Controller/DMA Controller . This will provide the high level architecture of the DMA and how it is hooked into the CPU memory system. The DMA on the C6202B has...
    on Dec 21, 2008
  • Forum Post: why DSP_fft16x16t let my program run to dead?

    Rolan Tang Rolan Tang
    Hi, my project is using C6416T, the FFT function DSP_fft16x16t fr. dsp64x.lib is called by my program , when I use optimization level -o2, the my dsp program will run to dead. But when I drop the optimization level to O0 or DSP_fft16x16t isn't called,my dsp program will run well. Can anybody help...
    on Jan 3, 2009
  • Forum Post: Re: why DSP_fft16x16t let my program run to dead?

    Rolan Tang Rolan Tang
    Hi Haryy, Thank you for your reply! I use the CCS 3.3 with the newest update 3.3.8.1, the optimization level is -o2(some files related to EMIFA access is O1),speed more cratical,no program level optimisation,others are default. The file using DSP_FFT16X16T is set to -O0. By the way, DSP/BIOS is used...
    on Jan 6, 2009
  • Forum Post: Problem while running dm6437_demo

    cang_rong cang_rong
    Dear Sir, my DM6437EVM is well but I have one problem with dm6437_demo. I installed CCStudio3.3.38.2, DM6437_DVDP_setupwin32_1_00_00_19.exe and TDS6437EVMboards_setup.exe all at C:, configured Setup CCStudio v3.3 and open CCStudio3.3. File->Load Program->dm6437_demo, display at screen is shaking...
    on Jan 14, 2009
  • Forum Post: C6000 updates for Code Generation Tools

    SteveM SteveM
    It seems that for each new update for C6000-CGT it get more difficult to download the file from the Update advisor webpage. I'm trying to download v6.1.7 at the moment and I can't get a response from the server. I can download earlier versions (e.g. v6.0.3) just fine. Has anyone else observed...
    on Jan 16, 2009
  • Forum Post: Re: FFT problem in 6713

    TKC TKC
    Hi Brad shouldn't the br_table be of sqrt(n) size rather than n? ~Nishank
    on Feb 10, 2009
  • Forum Post: [C6713] Creating Stream on a DHL-Object Fails

    Robert9862 Robert9862
    My application should be able to run in two modes. In the "codec mode", I use the following DSP/BIOS objects: A mini-driver for the AIC23 codec (configured in the tcf-file) A DIO adapter (configured in the tcf-file) A stackable overlap driver (DOV) for the input stream (configured...
    on Feb 25, 2009
  • Forum Post: DSP/BIOS Flash Boot for C6424

    Umberto Amadei Umberto Amadei
    I read the post kindly provided by Bernie Thompson ( http://community.ti.com/forums/t/3679.aspx ) about flash boot for C6424. I tried to download on my flash the example code (led.hex) provided in the attached zip file and all is OK. Then I tried to download my hex boot code generated by HexAIS_C642x...
    on Mar 10, 2009
  • Forum Post: Re: Out of Memory error using Code Composer Studio

    Enrico Zschau Enrico Zschau
    Hello Harry, i have the same problem. I'm using some parts of the boost-library (www.boost.org) in my project. The library can be compiled, but when trying to compile some examples (e.g. from serialization), the linker aborts after some time with the out of mem. message mentioned above. It...
    on Mar 11, 2009
  • Forum Post: I2C doesn't generate STOP condition

    Robert9862 Robert9862
    I am using the I2C module in master mode with RM=1 (repeat mode). The communication should look like this: START (r/w=0) send some bytes to the slave RESTART (r/w=1) receive one byte from the slave STOP Everything works fine (the bus analyzer shows that all data is transmitted and received...
    on Mar 12, 2009
  • Forum Post: McBSP Interrupt configuration for TMS320c6414T ,extarnal Frame sync for receiving and transmitting

    dspguy_78 dspguy_78
    Hi All, Currently I am working on the DSP TMS320C6414T , configuring McBSP serial interrupts to CPU (not using EDMA purposely ). MCBSP 0 having interrupts as following Intr 5 => McBSP0 Transmit == > transmit data to Backplane (exchange interface) Intr 6 => McBSP0 Receive == > receive...
    on Mar 13, 2009
  • Forum Post: I2C first byte transmission problem with TMS320C6720

    J.F Gagnon J.F Gagnon
    Hi! I am working on an electronic drum as a final school project and we are using the TMS320C6720. Right now , i am working on the I2C and i have a problem. Whenever i begin a transmission, i always get a dummy byte sent first (0x00) even though i set the first byte to be 0x40 ( write address of the...
    on Mar 24, 2009
  • Forum Post: Re: request for help... it is very urgent...please help....

    MANIKANDAN NAGARAJAN MANIKANDAN NAGARAJAN
    first i thank u buddy for your reply.... that error was from matlab only....it displayed as "Embedded matlab block do not support continuous sample time blocks"(From workspace)....{NOTE:This error was shown only during building process while i was trying to implement my algorithm in dsk 6416...
    on Apr 5, 2009
  • Forum Post: sprintf,printf and %f,%g,%e not working

    Douglas Corarito Douglas Corarito
    I'm using sprinf and printf in multiple threads in my app. RTS functions appeared to be working fine until I called: char[128] buffer = { '\0' }; float fpVar = 1.0; sprintf( buffer, "%f", fpVar ); Which did nothing. Has anyone gotten %f,%g,%e format specifiers to work...
    on Apr 23, 2009
  • Forum Post: Re: Memory allocation

    RandyP RandyP
    Welcome to the world of DSP. The first program is always a fun learning curve, so I applaud you for starting with something simple like this, which is slightly easier than a "Hello, world!" app. You will have a Technical Reference document for your C6211 development board; usually it comes...
    on May 13, 2009
  • Forum Post: Re: Memory allocation

    Geoffroy Rivet-Sabourin Geoffroy Rivet-Sabourin
    I have found the the memory map for the C6211 board. I use this .cmd file mostly from a TI example. -c -heap 0x500 -stack 0x500 /* very large stack for DSP programs. */ -lrts6200.lib MEMORY { vecs: o = 00000000h l = 00000200h I_HS_MEM: o = 00000200h l = 00000020h IRAM: o = 00000220h l = 0000FDE0h...
    on May 15, 2009
  • Forum Post: Re: Memory allocation

    BrandonAzbell BrandonAzbell
    The memory declaration is not CEO (as in the letter O), but CE0 (as in the number zero). Please modify your linker command file to the following for allocating .sysmem. .sysmem > CE0
    on May 15, 2009
  • Forum Post: HELP! 6727 DSP/BIOS how to simulate a Hardware Interrupt(HWI)?

    yang guo yang guo
    my program is like this: #include "Configuration1cfg.h" #include"hwi.h " void main() { HWI_enable(); LOG_printf(&LOG0,"jjjjjjj"); } void HWI_int555() { LOG_printf(&LOG0,"bbbbbbb"); } I config the DSP/BIOS and connect the pin. But the interrupt...
    on Jul 29, 2009
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use