This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Touch screen isn't working in ICS on beagle board xm

Hi,

We are trying to bringup android ics on beagle board XM using the steps mentioned in http://code.google.com/p/rowboat/wiki/ICSonBeagleboard_WithSGX . We could bringup the ICS Home screen with few modifications in kernel configuration and video driver changes as mentioned in http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_PortingGuides. But the touch screen isn't working. We have made some modification in touch-screen (ADS7846) driver as mentioned in http://e2e.ti.com/support/embedded/android/f/509/t/165103.aspx#605225 and http://e2e.ti.com/support/embedded/android/f/509/t/163475.aspx#600215.

We are using the boot argument as following:

setenv bootargs 'console=ttyO2,115200n8 androidboot.console=ttyO2 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext3 rootdelay=1 init=/init ip=off omap_vout.vid1_static_vrfb_alloc=y vram=24M omapfb.vram=0:24M omapdss.def_disp="dvi" omapfb.mode=dvi:800x480MR-24'

We are using the development Beagle-XM RevC board from chipsee.

Can you please help us bringing up the touch screen.

Regards

Georji

7 Replies

  • Hi,

    Are you getting any events from touch driver.

    $getevent

    also see if touch driver is registered to input subsystem

    $getevent -p

    BR,

    satish

    Kindly click the verify answer button on this post if it answer your question.

  • In reply to Satish Patel:

    Hello Satish,

    Thanks for your reply. We tried executing this command and for $getevent we saw that the Touch device is registered to input sub-system. But whne we did $getevent -p and we touched the screen, we didn't get any events from the device. We tried to configure the SPI, using the link http://elinux.org/BeagleBoard/SPI#Configuring_Pinmux but we had no luck on this.

    I have attached the board file and ads7846 driver code for your reference.

    Can you please let us know what else we need to do to make the Touch Screen driver working?

    Thanks,

    Georgi.

  • In reply to Georji Ghosh:

    Hi Georgi,

    1. I can not find any attachment in the thread. Could you repost the same ?

    2. Which kernel are you using ?

    3. Are you calling - input_report_abs from your driver, to send events to input subsystem.

     

    BR,

    satish

    Kindly click the verify answer button on this post if it answer your question.

  • In reply to Satish Patel:

    Hi Satish,

    Thanks for your quick response.

    I have attached the board file and ads7846 driver code for your reference along with dmesg kernel log once again.

    1016.files.zip

    We are using 2.6.37 kernel.

    Yes I can see that  input_report_abs call from ads7846 touch driver, to send events to input subsystem but in dmesg log I didn't find any log.

    Please let me know i had done something wrong.

    Regards

    Georji

  • In reply to Georji Ghosh:

    Hi Georji.

    Are you getting any touchscreen interrupts?

    Please post output of following command to debug this further.

    #cat /proc/interrupts

    Regards,

    Pankaj Bharadiya

    PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

  • In reply to Pankaj Bharadiya:

    Hi guys!

    I have exactly the same state. Could we figure out this thing because I have listed the touch controller in getvent -p, I can see it is recognized in dmesg but the getevent doesn't show any events... I think this is really close to work it out because if I remove the spi_register_board_info stuff then the ads7846 device is not recognized by the kernel so the SPI communication is ok.

    Another thing about I'm not sure and an explanation from some skilled jedi would be very welcome :) is the display thing. If I understand right the current TI kernel branch for the android ics only has tv and dvi support  in board-omap3beagle.c file. However the video signal is still pushed to the LCD. I understand this as a fallback and that the resolution and the density can be still configured with kernel boot args, but the pro way will be to implement the lcd_enable init, disable stuff like at board-omap3evm.c, am I right? What is the proper way to drive a third party lcd and to use only lcd, is there a tutorial explaining this? The main reason why I don't understand this is that the board-omap3beagle.c file does not have any lcd related stuff and the panel is still working as I wrote it...

    Guys please help work this out so we can make the patches available for all of you who need them.

    Thanks in advance,

    sodjas

  • In reply to sodjas:

    Hi!

    Some additional information.

    • So the basis is that the SPI channel is established because we see:

    spi3.0 supply vcc not found, using dummy regulator <---- Can this be a problem?!?!?!

    ads7846 spi3.0: touchscreen, irq 317

    input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.3/spi3.0/input/input1

    • getevent dumps the following:

    root@android:/ # getevent -p

    could not get driver version for /dev/input/mice, Not a typewriter
    add device 1: /dev/input/event1
    name: "ADS7846 Touchscreen"
    events:
    KEY (0001): 014a
    ABS (0003): 0000 : value 0, min 0, max 4095, fuzz 0, flat 0, resolution 0
    0001 : value 0, min 0, max 4095, fuzz 0, flat 0, resolution 0
    0018 : value 0, min 0, max 255, fuzz 0, flat 0, resolution 0
    input props:
    <not available

    could not get driver version for /dev/input/mouse0, Not a typewriter
    add device 2: /dev/input/event0
    name: "gpio-keys"
    events:
    KEY (0001): 0114
    input props:
    <not available

    add device 3: /dev/input/event2
    name: "twl4030_pwrbutton"
    events:
    KEY (0001): 0074
    input props:
    <not available

    I bet there is some problem with the interrupt system.

    • Another interesting thing is the omap based gpio handling:

    // omap_set_gpio_debounce(OMAP3_BEAGLE_TS_GPIO, 1);
    // omap_set_gpio_debounce_time(OMAP3_BEAGLE_TS_GPIO, 0xa);
    gpio_set_debounce(OMAP3_BEAGLE_TS_GPIO, 310);

    The first two lines threw linking error with the beagle step. I googled and found out that the third line with common gpio lib is a workaround at panda board. Could it be possible that the common gpio differs from the platform specific one? I saw that the c files are there they're just simply not compiled? Can I check it in kernel config? If yes where?

    Best Regards,

    sodjas

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.