This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Queries regarding hardware cryptographic accelerators in DM8148.

Hi,

I have two queries regarding hardware cryptographic accelerators in DM8148, which are as follows

1 . Dose the DM814x Crypto API Driver (Linux drivers that provide access to the hardware cryptographic accelerators) supports rijndael (with block size of 192) ?.

2. Is there any documentation avilable for hardware cryptographic accelerators usage/programming ,for dm8148 platform?

Following are my setup details:-

sdk:- ezsdk 5_03_01_15

platform :- dm8148

patch:- NSS-Crypto-driver-software-beta-0.9.patch.gz applied