This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Jelly Bean porting on Panda Board

Hi,

   We formated the SD card as fat32 which contains the MLO,U-boot.bin and uImage(3.5 Linux kernel) and as ext3 which is having Jelly Bean File system.

   We took    Linux kernel version 3.5 from mainline linux git and linux kernel is compiled with tool chain Sourcery G++ Lite 2010q1-202 . We compiled the Jelly Bean 

   source as procedure available in the link http://source.android.com/source/building.html .

   We are getting the following error   with  Panda board while when we  tried for booting jelly bean File system (zoom).  

Error:

[    5.189758] init: skipping insecure file '/default.prop'
[    5.198059] init: skipping insecure file '/init.rc'
[    9.516693] init: Timed out waiting for /dev/.coldboot_done
[    9.532562] init: skipping insecure file '/system/build.prop'
[    9.544921] init: Unable to open persistent property directory /data/property errno: 2

Complete Log is also provided. 

4263.Logfile.txt

Please help us on this.


Thanks & Regards

Bhimesh


  • In reply to Huy-Tinh Nguyen:

    Hello

    I booted my pandaboard es by below way. But below URL has not source but only images to boot. May help you!

    https://android-build.linaro.org/builds/~linaro-android/panda-jb-gcc47-tilt-stable-blob/  

  • In reply to chao wu1:

    Thanks for your reply. But I'm finding source for Jelly Bean-Pandaboard. I'v done follow this link :http://omappedia.org/wiki/4AJ.1.1_OMAP4_Jelly_Bean_Release_Notes#Introduction. but not success because This source is responsible to Blaze tablet not Pandaboard and I dont have Patch file for Panda too (Like this link: http://omappedia.org/wiki/4AI.1.4_OMAP4_Icecream_Sandwich_Panda_Notes). So Who has successed with Building JB Panda or has Guide for building this? Please give me. Thanks so much.

    NHT.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.