Hi ,
I am using Android ICS 4.0.3 and target is custom blaze board. I want to use NFC chip set . I built the kernel with NFC enabled, but in the android stack i did not get any HAL layer for NFC. I searched under the path
/Android/device/ti/blaze_tablet/libsensors.
can any body tell me where to get the Hardware abstraction layer code for NFC .
Thanks in advance,
Kiran.
hi kiran,
can you tell me how to buld the kernel with nfc enable??
Regards
Hi dibin,
Procedure to build the kernel with nfc
[1] using tools menu config or xconfig slect your nfc chip set . you can enable your nfc chip as part of kernel or external module.
[2] once your .config file is updated with nfc support, give make command to compile the kernel
i.e,. make ARCH=<your architecture> uImage
Note:
[1] Before you proceed to do make ,dont forget to set your cross compile variable and path to to cross compiler in environment variable PATH.
[2] If you are building the nfc as external moudle , after step 2, type the below command
make ARCH=<your architecture> modules
The above command will generate the nfc module (*.ko) under your drivers/nfc/<chip_name/ folder
dibin
Hi Kiran,
thanks for your response, i am using TI Android ICS 4.0.3 DevKit 3.0.0 sources for image building, and i don have any kernel/drivers/nfc directory
do 2.6.37 kernel support nfc , can i download the driver and insmod it ?
thanks in advance
Regards,