Hi,
I built the below pandaboard build from the wiki page.
http://omappedia.org/wiki/Building_L27.IS.2.M1_for_PandaBoard,_with_USB_camera_support
I have having the following issue:
1) In the status bar i get the error " No Internet Connection", so i am not able to access any webpages.
2)But I can ping to different IP's from Board and viceversa, so ethernet is up and my board has got an dhcp ip.
3)I tried enabling the Wifi, but it gets stuck. But this is listed as a known issue in wiki page.
I need help in enabling internet on this build.
Best Regards,
Aldon