Hi,
We formated the SD card as fat32 which contains the MLO,U-boot.bin and uImage(3.5 Linux kernel) and as ext3 which is having Jelly Bean File system.
We took Linux kernel version 3.5 from mainline linux git and linux kernel is compiled with tool chain Sourcery G++ Lite 2010q1-202 . We compiled the Jelly Bean
source as procedure available in the link http://source.android.com/source/building.html .
We are getting the following error with Panda board while when we tried for booting jelly bean File system (zoom).
Error:
[ 5.189758] init: skipping insecure file '/default.prop'
[ 5.198059] init: skipping insecure file '/init.rc'
[ 9.516693] init: Timed out waiting for /dev/.coldboot_done
[ 9.532562] init: skipping insecure file '/system/build.prop'
[ 9.544921] init: Unable to open persistent property directory /data/property errno: 2
Complete Log is also provided.
Please help us on this.
Thanks & Regards
Bhimesh