Hi
After building android ics for pandaboard there is no camera application in the menu i follwed TI omap docuement.
I need ics defalult camera APK please send me the default apk for the ICS pandaboard.
Thanks and regards
Maqsood khan
Maqsood,
Please mention the release used for this. Is it http://omappedia.org/wiki/4AI.1.4_OMAP4_Icecream_Sandwich_Panda_Notes?
Regards,
Chintan
------------------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.------------------------------------------------------------------------------------------------------------------
Hi Chintan/Maqsood,
Can you please suggest most stable android ICS release for Pandaboard/Pandaboard-ES?
It must have support for Camera, hw encoder decoder, ethernet, NFS booting (preferred for development).
There are so many releases on the internet but non of them looks stable and promising for the feature I am looking for.
Krunak
Hi Chintan,
I am having same issue.
I am testing in the following software and hardware environment: OS Kernel : Linux® 3.0Android : Android IcecreamSandwich 4.0.4(MR1.1)Toolchain : CodeSourcery compiler version Sourcery G++ Lite 2010q1-202 for ARM GNU/LinuxReference hardware platforms : PANDA BOARD REV A2Build Host OS : Ubuntu 11.10Android ICS Release : 4AI.1.4 OMAP4 Icecream Sandwich Panda (http://omappedia.org/wiki/4AI.1.4_OMAP4_Icecream_Sandwich_Panda_Notes)
Can you please suggest me stable release ?
Best Regard's
BK