This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

BeagleboneBlack android filesystem compile issue

Hi all,

I am facing compiling error with jellybean filesystem for beaglebone black.

The source code is downloaded from rowboat following this manual- http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide

Java version used- jdk1.6.0_45,  and host machine is ubuntu12.04 (64-bit) on virtual box.

Could anyone please help me solve this.

Command -make TARGET_PRODUCT=beagleboneblack OMAPES=4.x -j4

Error message while compiling-

host Executable: bcinfo (out/host/linux-x86/obj/EXECUTABLES/bcinfo_intermediates/bcinfo)
host SharedLib: libdvm (out/host/linux-x86/obj/lib/libdvm.so)
Install: out/target/product/beagleboneblack/system/lib/libssl.so
Install: out/host/linux-x86/bin/dasm
host Executable: dexopt (out/host/linux-x86/obj/EXECUTABLES/dexopt_intermediates/dexopt)
host Executable: dictTest (out/host/linux-x86/obj/EXECUTABLES/dictTest_intermediates/dictTest)
host Executable: grxmlcompile (out/host/linux-x86/obj/EXECUTABLES/grxmlcompile_intermediates/grxmlcompile)
Install: out/host/linux-x86/bin/llvm-dis
Install: out/host/linux-x86/bin/llvm-ndk-link
Install: out/host/linux-x86/bin/llvm-rs-link
Install: out/host/linux-x86/bin/mksnapshot.arm
host Java: smali (out/host/common/obj/JAVA_LIBRARIES/smali_intermediates/classes)
collect2: ld terminated with signal 9 [Killed]
make: *** [out/host/linux-x86/obj/EXECUTABLES/clang_intermediates/clang] Error 1
make: *** Waiting for unfinished jobs....
Note: Some input files use unchecked or unsafe operations.
Note: Recompile with -Xlint:unchecked for details.

Regards,

Ebin

  • Hi Ebin,

    Can you run the build command with -j1 and get the exact error?

    Can you also check the available disk space?

    Regards,

    Arun

    If this post answers your query, consider clicking Verify Answer

  • In reply to Arun Joseph:

    Hi Arun,

    Thanks for the reply,

    Filesystem compiled successfully with the build command- make TARGET_PRODUCT=beagleboneblack OMAPES=4.x -j1

    I found a difference in the boot up message when compared with precompiled image boot messages-

     For precompiled image [    0.000091] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)

    and for the image i compiled its [    0.000183] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320) .

    Will this affect any functions of the board?

    Regards,

    Ebin

  • In reply to ebin jose:

    Hi Ebin,

    The MPU frequency 1GHz is enabled on A5A, A5B and A5C. Which is the version of the BeagleBone Black you are trying?

    Can you check if the compiled MLO/u-boot and uImage commit ids are latest from the rowboat? Also can you copy the complete dmesg till this print?

    Regards,

    Arun 

    If this post answers your query, consider clicking Verify Answer

  • In reply to Arun Joseph:

    Hi Arun,

    I am using beaglebone black version A5C.

    Console messages at bootup-

    U-Boot SPL 2013.04-dirty (May 20 2013 - 14:30:06)
    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Peripheral mode controller at 47401000 using PIO, IRQ 0
    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Host mode controller at 47401800 using PIO, IRQ 0
    OMAP SD/MMC: 0
    mmc_send_cmd : timeout: No status update
    reading u-boot.img
    reading u-boot.img


    U-Boot 2013.04-dirty (May 20 2013 - 14:30:06)

    I2C:   ready
    DRAM:  512 MiB
    WARNING: Caches not enabled
    NAND:  No NAND device found!!!
    0 MiB
    MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
    *** Warning - readenv() failed, using default environment

    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Peripheral mode controller at 47401000 using PIO, IRQ 0
    musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn)
    musb-hdrc: MHDRC RTL version 2.0
    musb-hdrc: setup fifo_mode 4
    musb-hdrc: 28/31 max ep, 16384/16384 memory
    USB Host mode controller at 47401800 using PIO, IRQ 0
    Net:   <ethaddr> not set. Validating first E-fuse MAC
    cpsw, usb_ether
    Hit any key to stop autoboot:  0
    gpio: pin 53 (gpio 53) value is 1
    mmc0 is current device
    micro SD card found
    mmc0 is current device
    gpio: pin 54 (gpio 54) value is 1
    SD/MMC found on device 0
    reading uEnv.txt
    214 bytes read in 4 ms (51.8 KiB/s)
    Loaded environment from uEnv.txt
    Importing environment from mmc ...
    Running uenvcmd ...
    reading uImage
    4178800 bytes read in 505 ms (7.9 MiB/s)
    ## Booting kernel from Legacy Image at 81000000 ...
       Image Name:   Linux-3.2.0-00244-gcf99001
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    4178736 Bytes = 4 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    [    0.000000] Linux version 3.2.0-00244-gcf99001 (root@ebin-VirtualBox) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 Sat Aug 3 01:24:27 IST 2013
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine: am335xevm
    [    0.000000] Memory policy: ECC disabled, Data cache writeback
    [    0.000000] AM335X ES2.0 (sgx neon )
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
    [    0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=512M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off
    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Memory: 512MB = 512MB total
    [    0.000000] Memory: 509880k/509880k available, 14408k reserved, 0K highmem
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    [    0.000000]     vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    [    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc078a000   (7688 kB)
    [    0.000000]       .init : 0xc078a000 - 0xc07e0000   ( 344 kB)
    [    0.000000]       .data : 0xc07e0000 - 0xc084ba70   ( 431 kB)
    [    0.000000]        .bss : 0xc084ba94 - 0xc09a3890   (1376 kB)
    [    0.000000] NR_IRQS:396
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [    0.000000] Total of 128 interrupts on 1 active controller
    [    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
    [    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
    [    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 13                                                                     1071999ms
    [    0.000000] Console: colour dummy device 80x30
    [    0.000152] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320)
    [    0.048706] pid_max: default: 32768 minimum: 301

    Regards,

    Ebin

  • In reply to ebin jose:

    Hi Ebin,

    The MLO and u-boot time stamps looks so old - May 20.

    Can you check two things

    1) Are you holding the switch near uSD card to load boatloader from uSD?

    2) Try with the latest MLO and u-boot.img

    Regards,

    Arun

    If this post answers your query, consider clicking Verify Answer

  • In reply to Arun Joseph:

    Hi Arun,

    Thanks for reply.. it worked with holding the switch s2 and booting.

    Regards,

    Ebin

  • In reply to Arun Joseph:

    hi Arjun,

    I tried the command with -j1 on ubuntu 12.04 and got the same error.

    Can you please help me.

    Regards,

    Shyam

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.