Hello all, I've an AM335x board with Android 4.1.2 and a MU609 Huawei GPRS/GSM
module.
When start up, the USB will see the module as 5 tty serial ports:
[ 9.097778] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[ 9.250244] usb 1-1: New USB device found, idVendor=12d1, idProduct=1573
[ 9.257354] usb 1-1: New USB device strings: Mfr=5, Product=4, SerialNumber=0
[ 9.264892] usb 1-1: Product: HUAWEI Mobile
[ 9.269317] usb 1-1: Manufacturer: Huawei Technologies
[ 9.279113] cdc_ether 1-1:2.0: eth1: register 'cdc_ether' at usb-musb-hdrc.1-1, CDC Ethernet Device, 00:a0:c6:03:81:30
[ 9.291595] option 1-1:2.2: GSM modem (1-port) converter detected
[ 9.298522] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0
[ 9.306488] option 1-1:2.3: GSM modem (1-port) converter detected
[ 9.313323] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1
[ 9.321197] option 1-1:2.4: GSM modem (1-port) converter detected
[ 9.327972] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2
[ 9.335815] option 1-1:2.5: GSM modem (1-port) converter detected
[ 9.342620] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB3
[ 9.350494] option 1-1:2.6: GSM modem (1-port) converter detected
[ 9.357208] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB4
The relevant ports are:
ttyUSB0 is used for sending AT command
ttyUSB3 is used for getting GPS NMEA strings
ttyUSB4 is used for sending AT commands to GPS
ttyUSB1 and ttyUSB2 are used for debug or other sftuffs...
If the modem stops to works, we have to disconnect it to the system turning it off
via GPIO pin...
when we turn on the module again, the enumeration of the tty USB will change:
[ 63.169250] usb 1-1: new high-speed USB device number 3 using musb-hdrc
[ 63.311859] usb 1-1: New USB device found, idVendor=12d1, idProduct=1573
[ 63.318878] usb 1-1: New USB device strings: Mfr=5, Product=4, SerialNumber=0
[ 63.326354] usb 1-1: Product: HUAWEI Mobile
[ 63.330749] usb 1-1: Manufacturer: Huawei Technologies
[ 63.353393] option 1-1:2.2: GSM modem (1-port) converter detected
[ 63.360382] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0
[ 63.368194] option 1-1:2.3: GSM modem (1-port) converter detected
[ 63.374908] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1
[ 63.382568] option 1-1:2.4: GSM modem (1-port) converter detected
[ 63.389190] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2
[ 63.396881] option 1-1:2.5: GSM modem (1-port) converter detected
[ 63.403533] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB4
[ 63.411163] option 1-1:2.6: GSM modem (1-port) converter detected
[ 63.417816] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB5
[ 83.155975] cdc_ether 1-1:2.0: eth1: CDC: unexpected notification 01!
In this case, the ttyUSB3 is not more available and GPS application do not works...
There is a way to force the system to hold the original enumeration?
Thanks
M. Sangalli