Hi Everyone.
I have a question relating to getting a peripheral working on USB 1 on the AM335x Starter Kit. When I am booted into Android and I connect a mouse into USB 1 it works fine, but the moment I connect another peripheral into USB 1 such as a biometrics scanner or something like that, it just refuses to work.
The biometrics scanner I have has an Android application that was released as part of it's SDK, so I know it works. The USB 1 port seems to be powering the devices, but there is just not data being transferred. I am not sure if I am missing something somewhere?
Just a note, I am using a 5V 800mA power supply as it is the only thing I have, I have tried powering the biometrics scanner independently (so that USB 1 is not giving it power), but still I have no data. Could it be a power issue? It does not seem like it is since the attached device is powering up? Perhaps a setting somewhere that I am not aware of?
Thanks