I am having trouble getting Android to boot on custom hardware. The hardware design was based on the AM335x Starter Kit. The problem seems to be the MLO file. The u-boot.img that I created will boot on the starter kit when the MLO file for the starter kit is used. When attempting to use the MLO file that I created using the mux.h and pinmux.h r hardware guys neither the custom board or the dev kit will boot. The custom board will not boot using the MLO file for the dev kit.
Does anyone have any suggestions?