Hello All,
We are facing issue of binder transaction failed error on AM3352 Customized board.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
We are facing issue of binder transaction failed error on AM3352 Customized board.
Hello Team,
First of all ,i am grateful to you for your response.
I reproduced the issue on Beaglebone board.Simply compiled
by make droid option mentioning the product name as beaglebone and ported the code over the board.
The same error comes over beaglebone also.
I am using Ubuntu 12.04(64bit) PC.
We have 256 MB Nand and DRAM 512 MB on our customized AMM3352 board.
The above errors continously comes on console.
Regards
Nitish Mehta
Hi Nitish,
Thanks for your reply. I'm not sure to understand what is meant by "ported the code over", have you made modifications to the original BSP before trying on the Beaglebone? Could you confirm that this binder error does not happen when using the pre-built binaries?
We couldn't reproduce the issue here, can you explain it a bit more, when does it happen exactly? Do you see the Launcher? Are you able to start applications? As for your first post, mediaserver needs to be started from init otherwise the system won't work.
Hi Nitish,
Thanks for the feedback. Please try with the following pre-built binaries for the beaglebone:
Hello Team,
First of all i am extremely sorry for the late reply.
I used the prebuilt binary for the beaglebone board.
Here are the following observations :
On 1st Boot :
Binder transaction error came only one time.
On 2nd Boot :
When bootanimation exits crashes were observed.I am attaching
logs heading "jb_2nd_boot"
On 3rd Boot:
Systems runs no above errors were found.I am attaching log heading "jb_3rd_boot"
Also i have tused the file system binary for our board also.But it doesnt support sgx.
So,after mount of rootfs crashes were observed.
Note:I have used it for beaglebone board and we dnt have lcd cape.
So,this observations are from console logs.
Please guide me in this to proceed further for my customized board AM3352.
Regards
Nitish Mehta
###################################################################################################
[Log Deleted]
##################################################################################################