A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How can i use WiLink8 wifi adapter in TI_Android_JB_4.2.2_DevKit_4.1.1 SDK ?
Other Parts Discussed in Thread: WL1831Hi,
I've a custom board which designed from AM335x Starter Kit. I will use these board in Oven and dishwasher projects as an advanced HMI module.
So I have made many customizations for my own needs and almost all of them except wireless connectivity work properly.
I used JORJIN WG7831-D0 module (which includes a TI WL1831 SoC) instead of existing WiLink7 module.
I made pin-mux operations thoroughly. But later I could not succeed in driving WL18xx module.
I tried to follow "WL18xx System Build Scripts" document (processors.wiki.ti.com/.../WL18xx_System_Build_Scripts) but it is explained for Linux SDK and things gets complicated when createing setup-env file.
Does the default TI_Android_JB_4.2.2_DevKit_4.1.1 SDK include necessary driver for WL18xx modules?
Or should I have to create compat.ko, wl18xx.ko, wlcore.ko, wlcore_sdio.ko, mac80211.ko, cfg80211.ko files?
if the answer is yes how can I make it for TI_Android_JB_4.2.2_DevKit_4.1.1 SDK?
I will be very happy for any suggestion, answer etc.
Regards
Mehmet