This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I additionally get the following error logs when I run the makefile under "/kernel/hardware/ti/wlan/mac80211/compat_wl12xx" directory in kernel.
mehmet@kickoff:~/mydroid/hardware/ti/wlan/mac80211/compat_wl12xx$ make
/home/mehmet/mydroid/hardware/ti/wlan/mac80211/compat_wl12xx/config.mk:256: "WARNING: CONFIG_CFG80211_WEXT will be deactivated or not working because kernel was compiled with CONFIG_WIRELESS_EXT=n. Tools using wext interface like iwconfig will not work. To activate it build your kernel e.g. with CONFIG_LIBIPW=m."
make -j1 -C /kernel M=/home/mehmet/mydroid/hardware/ti/wlan/mac80211/compat_wl12xx modules
make: *** /kernel: No such file or directory. Stop.
make: *** [modules] Error 2
What corrections should I make?
Regards
Mehmet Rıza ÖZ
I could compile .ko files using following terminal commands sequentially.
cd hardware/ti/wlan/mac80211/compat_wl18xx
make ANDROID_ROOT_DIR=/home/mehmet/mydroid/ CROSS_COMPILE=arm-eabi- ARCH=arm clean
make ANDROID_ROOT_DIR=/home/mehmet/mydroid/ CROSS_COMPILE=arm-eabi- ARCH=arm
make ANDROID_ROOT_DIR=/home/mehmet/mydroid/ CROSS_COMPILE=arm-eabi- ARCH=arm install
compat.ko
mac80211.ko
cfg80211.ko
wl1251.ko
wl12xx.ko
wl18xx.ko
wlcore.ko
wl1251_spi.ko
wlcore_spi.ko
wl1251_sdio.ko
wlcore_sdio.ko
files are created under "hardware/ti/wlan/mac80211/compat_wl18xx" directory
RegardsHi Mehmet,
Looks like you were able to compile. Thank you for sharing it here.