Hi all,
I am porting WiFi on a custom AM3352 board with TI-Android-JB-4.2.2-DevKit-4.1.1 for Product type as beaglebone. So far, I have successfully ported WIFI module and wifi works OK using command line wpa_cli and wpa_supplicant binaries.
When I Turn On the wifi from android's UI based settings, wifi drivers get loaded OK and I can have wlan0 interface up. I can also see the Wifi UI based setting showing Wifi is ON on the display.
I can scan, list and connect to APs using wpa_cli command in Android system.
Now, the problem is, when I turn the wifi ON from UI based wifi settings, it keeps showing me "Searching for Wi-Fi networks.." message and does not give the scanned results (Not sure if it is initiating scan process). I have waited for long time to get the screen updated with scanned APs, but it keeps on showing the same message.
As I have already checked the Wifi drivers with all possibilities, I need someone to help me to enable UI based access for scanning and selecting APs from WIfi settings in android 4.2.2.
Appreciate a response soon.
Regards,
Divyesh M