• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » Android » Android forum » All Tags » OMAP
Share
Android
  • Forum

Browse by Tags

Android

Welcome to the Android Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
OMAP
  • am3505/17_android
  • am3517
  • AM35xx
  • AM37X
  • android
  • Android ICS
  • Android OMAP Kernel
  • android rowboat
  • Beagle Board
  • beagleboard
  • beagleboard-xm
  • BeagleBoard-xM Android rowboat-dsp
  • booting
  • dm3730
  • DM37x
  • froyo
  • gingerbread
  • GingerBread_2_3_4_DevKit_2_1
  • ICS
  • kernel
  • LCD
  • OMAP OMAP35xx AM35xx AM3517 EVM
  • OMAP3530
  • rootfs build
  • rowboat
Related Posts
  • Forum Post: USB issue on Android

    haysam haysam
    I have a couple of EVM boards from Mistral (OMAP EVM Rev G board). I've built an SD card with the Android Froyo release. We are having an issue with the USB interface where it does not properly detect devices plugged into the port i.e. if I plug in a usb mouse (directly or thru a hub or a self...
    on Feb 8, 2011
  • Forum Post: How can I enable Android GUI to unlock SIM card after booting?

    Curtis Tu Curtis Tu
    Hi all, I had pored Froyo RIL to OMAP 3730. Those functions are OK (voice call, data call, sms...etc.) when SIM card status is "SIM_READY". But when the SIM card status is SIM_PIN (require PIN code to unlock SIM card), no GUI let me enter PIN code to unlock SIM card after booting, ...
    on May 17, 2011
  • Forum Post: Making the rootfs.tar.bz2 is very very slow in Android system build

    Eric tsui Eric tsui
    Hi, When I running the following commands: $ sudo ../../../../build/tools/mktarball.sh ../../../host/linux-x86/bin/fs_get_stats android_rootfs . rootfs rootfs.tar.bz2 The feedback is ../../../../build/tools/mktarball.sh: line 20: cd: android_rootfs: No such file or directory And then it...
    on Aug 2, 2011
  • Forum Post: Problem with Building Gingerbread from Sources to Beagleboard C4

    Juha Kamula Juha Kamula
    Hi, I'm currently trying to make a build from the sources and instructions(http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3-DevKit-1.0_DeveloperGuide) provided on TI's homepage. I've made a build that compiled and built without errors but it gets stuck on "Booting...
    on Aug 12, 2011
  • Forum Post: Android FroYo on OMAP35x boot but no display

    NuriaPazos NuriaPazos
    Hello everyone ! I have trouble with Android FroYo on OMAP35x. The system boot but there is no display except the boot logo despite that I can execute command via distant COM terminal. There are my spec's : I use TI_Android_FroYo_DevKit-V2.2 with source compiling / pre-built image and...
    on Nov 29, 2011
  • Forum Post: unable to build the devkit8000 gingerbread source code with dsplink

    devkit anonym devkit anonym
    Hi, I am trying to build the gingerbread source code for devkit8000 board. It is creating the system.img file in out/target/product/devkit8000. Then it is showing error while doing dsp-link. The error is as follows: Generated: (out/target/product/devkit8000/android-info.txt) Target system...
    on Dec 12, 2011
  • Forum Post: TI Android for medical devices

    Vasco Tesi Vasco Tesi
    Hi, we have to develop a medical device which is not life critical , but is class II and therefore has considerable reliability requirements. There are some platforms very attractive , like BeagleBoard and some others , which are low cost , powerful and with very rich connectivity. Is there...
    on Dec 21, 2011
  • Forum Post: Re: Configuring BeagleBoard's S1 User Button as Home Button in Android

    Faisal Hassan Faisal Hassan
    Hi, Check this header file <android-source>/bionic/libc/kernel/common/linux/input.h line no 87 for more key codes. Thanks, Faisal H
    on Mar 14, 2012
  • Forum Post: "omaplfb: OMAPLFB_Init: OMAPLFBInit failed" on am3517

    Kevin Chow Kevin Chow
    Hi, I am testing on custom board similar with am3517evm except LCD, I substitute a 7" LCD for 4"3' LCD. (7" LCD: 800*480, CLK=33300; 4"3' LCD: 480*272,CLK=9000) I am booting from NAND, and xloader, uboot, uImage, ubi.img are all on NAND, no MMC is attached. Each time...
    on Aug 12, 2011
  • Forum Post: TI Android 2.3.4 Camera Preview is skipping frame in random intervals

    ritesh raj ritesh raj
    Hi, I migrated from android froyo 2.2(linux kernel 2.6.32) to android 2.3.4 having linux kernel 2.6.37 , In froyo i was getting smooth display but in gingerbread as i am starting the camera preview i am facing frame skipping issue at random interval. I am using TI-Android-GingerBread-2.3.4-DevKit...
    on Mar 30, 2012
  • Forum Post: Android application (SIP client) not using RJ45 as default network interface on OMAP EVM board running Android ginger bread 2.3

    Ananth Kumar Srinivasan Ananth Kumar Srinivasan
    Hi, We are usng OMAP EVM board running Android 2.3 ( prebuilt images TI-Android-GingerBread-2.3.4-DevKit-2.1.). The board has RJ45 ethernet interface and does not have a Wifi module. When SIP client application is run on the board, it does not attempt to use RJ45 network interface to register to SIP...
    on Feb 6, 2012
  • Forum Post: OMAP4430 Clock speeds on Android

    Aldon Almeida Aldon Almeida
    Hello, I am having OMAP4430 based device which has Android ICS 4.0.3 on it. I have the following questions 1) I am trying to figure out the IVA-HD and DDR clocks at different operating point. But I am not able to find this information. Does anyone know how to get this information. 2) If anybody...
    on Jul 5, 2012
  • Forum Post: RE: DM3730: Video acceleration on Android ICS

    Dennis E Dennis E
    Hi Gary1, I am also trying to get DSP/Codec Engine functionality on OMAP3530 into our Android ICS systems. I have had no success finding any useful information for this endeavor. I have next to no experience with Gingerbread. Is there a website or a certain set of search terms I can use to find out...
    on Oct 31, 2012
  • Forum Post: Can u-boot used to boot Linux be used to boot a newly ported android Froyo kernel ?

    Donald Russell Donald Russell
    I would like to use the same hardware to boot either Linux or Android with only environment variable changes. Is Android dependent on any u-boot code not in a Linux u-boot build? Thanks
    on Aug 26, 2011
  • Forum Post: not able to boot android uImage-dirty

    kiran nayak kiran nayak
    hi all i build the rowboat-ics-2.37 kernel with some source code modifications then cross complied using arm-eabi- toolchain and got uImage-2.6.37-dirty image.. but while booting on beagleboard-xm ,it struck after below log messages ## Booting kernel from Legacy Image at 80300000 ... Image Name...
    on Nov 7, 2012
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use