Hello. I try to implement in the project code DSPLINK on side DSP. I use Code Composer Studio 4.2.4. Also I use a packet dsplink_linux_1_65_00_03.
At attempt to build the project I have following errors:
Severity and Description Path Resource Location Creation Time Iderrors encountered during linking; "client_dsp_dsplink2.out" not built client_dsp_dsplink2 line 0 1332317633774 2228unresolved symbol _DSPLINK_init, first referenced in ./main_Acoustic.obj client_dsp_dsplink2 line 0 1332317633773 2219unresolved symbol _NOTIFY_notify, first referenced in ./Acoustic_task.obj client_dsp_dsplink2 line 0 1332317633773 2220unresolved symbol _NOTIFY_register, first referenced in ./main_Acoustic.obj client_dsp_dsplink2 line 0 1332317633773 2221unresolved symbol _SMAPOOL_FXNS, first referenced in ./Acoustic_poolcfg.obj client_dsp_dsplink2 line 0 1332317633773 2222unresolved symbol _SMAPOOL_init, first referenced in ./Acoustic_poolcfg.obj client_dsp_dsplink2 line 0 1332317633773 2223unresolved symbol _ZCPYDATA_devObj, first referenced in ./aco_modcfg.obj client_dsp_dsplink2 line 0 1332317633774 2225unresolved symbol _ZCPYDATA_FXNS, first referenced in ./aco_modcfg.obj client_dsp_dsplink2 line 0 1332317633773 2224unresolved symbol _ZCPYDATA_init, first referenced in ./aco_modcfg.obj client_dsp_dsplink2 line 0 1332317633774 2226unresolved symbol _ZCPYDATA_tskFxn, first referenced in ./aco_modcfg.obj client_dsp_dsplink2 line 0 1332317633774 2227archive symbol directory is missing from archive "C:/ccs4/dsplink_linux_1_65_00_03/dsplink/dsp/export/BIN/DspBios/OMAPL138/OM APL138GEM_0/DEBUG/dsplink.lib" client_dsp_dsplink2 line 0 1332317633773 2213archive symbol directory is missing from archive "C:/ccs4/dsplink_linux_1_65_00_03/dsplink/dsp/export/BIN/DspBios/OMAPL138/OM APL138GEM_0/DEBUG/dsplinkdata.lib" client_dsp_dsplink2 line 0 1332317633773 2214archive symbol directory is missing from archive "C:/ccs4/dsplink_linux_1_65_00_03/dsplink/dsp/export/BIN/DspBios/OMAPL138/OM APL138GEM_0/DEBUG/dsplinkmpcs.lib" client_dsp_dsplink2 line 0 1332317633773 2215archive symbol directory is missing from archive "C:/ccs4/dsplink_linux_1_65_00_03/dsplink/dsp/export/BIN/DspBios/OMAPL138/OM APL138GEM_0/DEBUG/dsplinkmplist.lib" client_dsp_dsplink2 line 0 1332317633773 2216archive symbol directory is missing from archive "C:/ccs4/dsplink_linux_1_65_00_03/dsplink/dsp/export/BIN/DspBios/OMAPL138/OM APL138GEM_0/DEBUG/dsplinknotify.lib" client_dsp_dsplink2 line 0 1332317633773 2217archive symbol directory is missing from archive "C:/ccs4/dsplink_linux_1_65_00_03/dsplink/dsp/export/BIN/DspBios/OMAPL138/OM APL138GEM_0/DEBUG/dsplinkpool.lib" client_dsp_dsplink2 line 0 1332317633773 2218
Unfortunately, I cannot define a cause of error yet. Something not so with libraries. I hope that you will help me. Thanks.
The problem is decided. I once again built DSPLINK libraries. After that the program was compiled successfully.