***Parent thread is here --TH***I'm having similar problems with my TCF file. I had thing working and now the environment is broken. My TCF file is showing up in the Documents folder rather than in the DSP/BIOS Config folder. When I build, I get the message "Error, Don't know how to build file "C:\Projects\MyProject\Project.tcf"
Also I am unable to save my project because I get the error mesage 'Cannot save the project "C:\Projects\MyProject\Project.prj". Not all build tools are loaded"
I do get the graphical BIOS editor when I open my TCF file.
I'm running CCStudio 3.3. (About screen says 3.03)
Versions:
IDE 5.98.0.393
BIOS 5.33.04 (About screen reports 5.33.03)
CGTools 6.1.9
Thanks,
Chris
Why do you have a "prj" file? It should be a "pjt" file. Please attach your pjt file for inspection if the above steps do not help.
For future issues it would be preferable to start a new thread and perhaps post a link referencing this thread.
---------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------
Chris,I've moved this post to the Code Composer sub-forum as this did not exist at the time of the last thread. Hopefully one of our CCS gurus can chime in...
-Tim
---------------------------------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------