• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » BIOS » BIOS forum » All Tags » C674x
Share
BIOS
  • Forum
  • Announcements

Browse by Tags

BIOS

Welcome to the BIOS Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
C674x
  • 6748
  • BIOS
  • BIOS 5
  • BIOS 6
  • BIOS/DSP
  • BIOS6
  • BIOSPSP
  • BIOSPSP_ENG
  • C64x+
  • C6747
  • C6748
  • ccs
  • CCS v4
  • CCSv4
  • code Composer studio
  • Codec Engine
  • DSP/BIOS
  • DSP/BIOS 5
  • EDMA3
  • IPC
  • IPC BIOS
  • OMAPl138
  • OMAP-L138
  • RTSC
  • SPI
Related Posts
  • Forum Post: BIOSPSP audio example for C674x

    Yan8622 Yan8622
    Hi, The audio example given in the C674x BIOSPSP package would stop running if the audio processing between SIO Rx and Tx takes too long. I think a better handling of this situation would be to skip the a few audio frames but without breaking anything. Any advice how to do that? Thanks
    on Mar 23, 2010
  • Forum Post: implementing sound-task into NDK-client-example

    Rico Schulze Rico Schulze
    Hello I am trying to give my audio-processing program some network functionality. To do so i implemented my source code, wich is based on the audio-example of the psp into the NDK-client example. compiling linking and executing works well, but while running the audio-Task the creation of the in- and...
    on Jul 26, 2010
  • Forum Post: Exception on OMAPL138

    Marc48067 Marc48067
    Hello, When I start a debug session with CCS4 the FIRST TIME after powering up the OMAPL138 Experimenter Kit, the C674x always gets an exception. The EXC_dispatcher in turn redirects processing to UTL_halt(). When I terminate the first debug session in CCS4 and start it again (without power cycling...
    on Aug 16, 2010
  • Forum Post: How to allocate different sections into a single section with .tcf file ?

    PENG HUANG PENG HUANG
    Hi, everyone, I'm using OMAPL138 with CCS3.3 and DSP/BIOS 5.32 to develop DSP side firmware. I met a problem while using tconf script to control the memory allocation. I create some BUF objects in .tcf file, for example: bios.BUF.create("BUF_SDRAM_00000008"); bios.BUF.instance...
    on Nov 4, 2010
  • Forum Post: Run an RTSC SWI example on OMAPL138

    GINNI GINNI
    Hi everybody, at the moment I am trying to get a working standalone version of the RTSC SWI template included in SYS/BIOS 6.30. I am using CCSv4.2. I made a new project file with the SWI example. When I am debugging the example everything is working as expected. After generating an AIS .bin...
    on Nov 23, 2010
  • Forum Post: DSPBIOS 5.41.xx How do I set timer 2 as sys tick clock - OMAP L138

    Chappell Chappell
    I would like to use timer 2 as the DSPBios sys tick clock (tasks) but have am unsure how to enable this. This is normally done from the CLK properties menu in the DSPBIOS config menu but only timer0 and timer 1 are selectable. I see the standard configuration file bios_6748 .tci loads the seed file 6748...
    on May 26, 2010
  • Forum Post: C6748 DSP UPP DSP/BIOS test example memory issues.

    Fahed Bashir Fahed Bashir
    Hi, I have working on UPP DSP/BIOS driver to get Data from ADC. I am using upp_dvr_test.pjt which is in loopback mode. I have modified it to work in Receive mode. everything works fine for very less number of sample captures, but as i increase the number of samples, processor halts, and I can,t...
    on Feb 15, 2011
  • Forum Post: SPI DMA timing

    Admar Schoonen Admar Schoonen
    Hi I'm using the Logic EVM with C6748 SOM and I'm investigating spi transfer. So far, I have spi working in dma mode. However, like a few others on this forum, I've noticed that there is quite a big delay between chip select and start of spi clock if CSHOLD is set. This delay is not present...
    on Mar 8, 2011
  • Forum Post: RTSC template from EZSDK for XGCONF?

    Lee Holeva Lee Holeva
    I'm in the process of learning how to program Codec Engine and iUniversal, but one thing that I still have not figured out is how XGCONF gets the information about the EVM to generate a template for a .cfg file. I'm using the c6a816x EVM and at present I have two disparate tools sets, one in...
    on Apr 15, 2011
  • Forum Post: USB on C674x

    JimD JimD
    Hi All, I'm looking at some various options regarding enabling USB on the C6745 / C6747. We're looking at streaming data continuously from the device to a PC at a rate of about 2 Mbit/s using bulk transfer. I've been looking at a couple of options:- The most obvious is to use the...
    on Apr 27, 2011
  • Forum Post: C674x DSP/BIOS UART Driver Timeout

    Mark Monson Mark Monson
    Hello, I am using the UART driver in the DSP/BIOS PSP (1.30.01) at 115.2 k baud. We have a UART packet protocol that I need to receive. The packet length can vary, but the format it always the same. Each field is a byte, except for the data | start | length | command...
    on May 18, 2011
  • Forum Post: Re: DMAN3 Address Translation for TI8168 DSP for ACPY3

    RV RV
    Any updates? Can anyone from TI confirm if they are seeing same issues with c674x DMA transfers not working when it is from/to DSP IRAM to/from DDR3 for Netra and Centaurus? This is with: codec-engine_3_21_00_13_eng framework-components_3_21_00_17_eng in EZSDK 5_01_01_80. When...
    on Jul 21, 2011
  • Forum Post: C6747 BIOS (v5.33.01) interrupt service table issue

    Michael Martin79873 Michael Martin79873
    Hello, I am currently working to integrate two programs that were given to me for the C6747. One of these used BIOS for ECM-controlled interrupts for an audio processing routine, and one did not use BIOS, with UART2, non-ECM-controlled interrupts. Because of their separate creation, they have separate...
    on Jul 22, 2011
  • Forum Post: How to enable the Mcbsp LoopjobBuffers

    Cecil Cecil
    I want to enable the MCBSP loopjob buffers but I don't know how to verify whether they are enabled. The main problem is that I am using mcbsp in SIO_ISSUE_RECLAIM mode with 4 tx and rx buffers. My Input/read buffers seem to work ok but after I issue all 4 tx buffers I am only able to reclaim one...
    on Jun 15, 2011
  • Forum Post: Re: USB CDC device driver for 6746

    Mona Gandhi Mona Gandhi
    Thanks for the reply Shanmuga. Does that mean TI does not provide VID/PID for this family of processors like it does for Stellaris and Sitara? Could you please tell me where this important piece of information is documented? TI does provide USB CDC class driver for Stellaris family. Can you please...
    on Aug 31, 2011
  • Forum Post: Re: USB CDC device driver for 6746

    Mona Gandhi Mona Gandhi
    Hi Shanmuga, How about using Sitara CDC driver of 6748 for 6746 ? Waiting for your comments.. Thanks, Mona Gandhi.
    on Sep 5, 2011
  • Forum Post: spi with edma example issue (pspdrivers_01_30_01)

    Nikolay Kokorin Nikolay Kokorin
    Hello! I'm trying to debug SPI with EDMA example for evmOMAPL137 platform (from pspdrivers_01_30_01\packages\ti\pspiom\examples\evmOMAPL137\spi\edma\). During program execution Printf_Log has messages: EDMA3 : edma3init() passed write is Enabled write is Enabled Data compare Failed...
    on Sep 1, 2011
  • Forum Post: C674x Register save on context switch

    1768011 1768011
    Hi! Is there a list of registers that need to be saved upon a context switch on a 674x DSP? Currently i do save these which seems to work: AMR CSR IRP A0-A15 B0-B15 The compiler handbook lists some more for the C6740 family: FADCR Floating-point adder configuration...
    on Sep 12, 2011
  • Forum Post: Problems with Gpio Driver Configuration

    Steve Kreyer Steve Kreyer
    Hi all, I've a problem with configuring the gpio driver package. I want to use this package together with the spi driver. I've used the configuration of the example application provided by the PSP package as a template and stripped it down to my needs. Now when running configuro it fails...
    on Sep 14, 2011
  • Forum Post: MEM_stat() states part of heap being used prior to MEM_alloc() being called

    barry mohan barry mohan
    Hi E2Er's We are developng DSP code on OMAPL138 experimenter board (CCS 4.2, windows 7 & BIOS 5_41_10_36) - also seen on We have IRAM configured in *.tcf as follows base = 0x11800000 len = 0x38000 create heap in this memory = TRUE heap size = 28000 enter a user defined...
    on Sep 8, 2011
  • Forum Post: Simulation is standing still

    christian bach christian bach
    Hello I have a TMS320DM8148 on a TMDXEVM8148BTA Evaluation Board and using a LAN560 JTAG Emulator to connect to the processors via the 20Pin JTAG Port. Sadly the profiling does not seam to be working with this setup. So, I tried to use the simulator for the profiling but that just doesn't do...
    on Sep 19, 2011
  • Forum Post: SYSBIOS IPC Server/Client via MessageQ

    christian bach christian bach
    Hello I have a TMS320DM8148 on a TMDXEVM8148BTA Evaluation Board and using a LAN560 JTAG Emulator to connect to the processors via the 20Pin JTAG Port. Based on the MessageQ Example in the CCS5.1 Environment I tried to write my own MessageQ Program which shall be a Server who's computing...
    on Sep 19, 2011
  • Forum Post: dmtimer frequency mismatch

    Jibin Scaria Jibin Scaria
    Hi all, I am trying to execute BIOS 6 task mutex example in ccsv5.1 in DM8148 EVM. I am getting following error [C674X_0] ti.sysbios.timers.dmtimer.Timer: line 1031: E_freqMismatch: Frequency mismatch: Expected 32768 Hz, actual: 1740139 Hz xdc.runtime.Error.raise: terminating execution Can...
    on Oct 12, 2011
  • Forum Post: SYS/BIOS using the Task Example (Seperate Config Project) and getting multiple memory link sections overlapping...

    Mike Geppert Mike Geppert
    I am using a 3rd party board and their examples work great. Now I want to build one of my own and use SYS/BIOS in the project (using Code Composer Studio 4.2.4.00033). The configuration package seems to have defined memory sections (given in SYSBIOS/System/Program under Available Memory Segments...
    on Nov 4, 2011
  • Forum Post: Using SPI1 and/or SPI2 as slave with TI814x

    Rene Wittmann Rene Wittmann
    Hello, Reading the SPI TRM for DM8xx, chapter 1.2.4.1, I see the following sentence: "In slave mode, enabling a channel that is not channel 0 has no effect. Only channel 0 can be enabled." Does that mean that SPI1 or SPI2 cannot be configured as SPI slave? Or does channel 0 not...
    on Oct 24, 2011
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use