The following is a brief on Configuration used:
Processor : DM365
U-Boot (April 2010 release) (Configuration : davinci_dm365_ipnc_config)
Linux Kernel version: 2.6.18
"nand_bbt: ECC error while reading bad block table" started coming when the Flash Size was increased from 32M to 64M
On 32M flash this error was never seen. Any help on this would be appreciated.
Thanks in Advance...
In general, we ask that you please post the full console log that contains the error, as in from power on until the last error message. This helps us to see what's going on in the system and to answer a few questions we might have. Thanks!
Please click the Verify Answer button on this post if it answers your question.
Thanks,
Tom