Hello,
I would like to have the ability to flash dm8168 without CCS. Is it possible ?
Regards,
Ran
Hi Ran
Go through these link
http://processors.wiki.ti.com/index.php/TI81XX_PSP_U-Boot#Flashing_U-Boot_without_CCS
Regards
AnilKumar
Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question. Thanks!
Hi Anil,
Thanks for the post. It means that if we want this feature(flashing without CCS) in the final board, we need to have the ability to change the boot register in hardware (with switch for example as done in the EVM). without that, the CCS must be used for flashing, am I right ?
Hi Ran,
Yes, switch is required (with out this switch how can we change the boot modes?) otherwise CCS is the only option we have
.
Thanks for the answer. I see that there is also a CCS free version in TI web page. What is the diffrenece between the free version and the other versions ? (What is the Limit on the free limited version). I ask the question because I want to use CCS just for flashing purpose.
Thank You,
Better open a new thread for this question in CCS forum
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81.aspx